Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Unexpected behavior of EAGLE layout editor
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 16 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 3145 views
  • Users 0 members are here
  • eagle 6.4.0 professional
  • Layout Editor
Related

Unexpected behavior of EAGLE layout editor

SMD111
SMD111 over 9 years ago

The problem I have is described in the attached images (they are zoom-able).

I have a finalized, fully routed design:

image

At some point I decided to add a new gate to the schematic, so I copy IC5 and paste it as IC9. Please note that no connections on IC9 have been made yet:

image

Simply placing this gate on schematic causes significant changes on the board. As you can see, multiple nets become ripped up, even the nets that have nothing to do with IC5 or IC9.

image

Is it possible to avoid this effect?

Thank you,

Sergey

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 9 years ago

    On 22/07/2017 3:35 a.m., SMD111 wrote:

    The problem I have is described in the attached images (they are zoom-able).

    I have a finalized, fully routed design:

     

      At some point I decided to add a new gate to the schematic, so I copy IC5 and paste it as IC9. Please note that no connections on IC9 have been made yet:

     

    Simply placing this gate on schematic causes significant changes on the board. As you can see, multiple nets become ripped up, even the nets that have nothing to do with IC5 or IC9.

     

    Is it possible to avoid this effect?

    Thank you,

    Sergey

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/225828

     

     

     

    Hi Sergey

     

    It's important to say which version of Eagle you are using.

     

    I use v7.7 (Win7)  and can demonstrate I don't have  your problem.

    Using the example Schem/Board Hexapod I can copy a device in the

    schematic and it appears without air-wires on the board, ready to be

    placed. The rest of the board remains unaltered.

     

    It may be the technique you are using to copy the part (ah! maybe the v8

    select mechanism has caught you out). I simply right click on the symbol

    (IC5) and select copy from the context menu. Then you will only have the

    IC stuck to the cursor and no nets connected to the pins.

     

     

    HTH

    Warren

    --

    ... use NNTP://news.cadsoft.de and a functional news reader like

    Thunderbird!

    ... or http://www.eaglecentral.ca browser access to CadSoft EAGLE

    support forums.

     

    ---

    This email has been checked for viruses by Avast antivirus software.

    https://www.avast.com/antivirus

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • SMD111
    0 SMD111 over 9 years ago in reply to autodeskguest

    Hi Warren, thank you for replying.

     

    I have EAGLE 6.4.0 Professional. It is old, but I like "good old" things :-)

     

    And for copying, I just select the copy mode on the toolbar, then click on the gate, then the IC is duplicated and stuck to cursor, then I place it with a click. After that I press "Switch to board" button and see airwires in some places where traces used to be.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to SMD111

    On 22/07/2017 8:14 a.m., SMD111 wrote:

    Hi Warren, thank you for replying.

     

    I have EAGLE 6.4.0 Professional. It is old, but I like "good old" things image

     

    And for copying, I just select the copy mode on the toolbar, then click on the gate, then the IC is duplicated and stuck to cursor, then I place it with a click. After that I press "Switch to board" button and see airwires in some places where traces used to be.

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/225833

     

     

    The problem could be the following if the board is from a version prior

    to v6.

     

    The following is copied from the release notes (UPDATE_en.txt) which

    comes with Eagle.

     

    • Supply layers:

     

      - Supply layers (i.e. layers with names that start with a '$') are no

    longer treated special. Layers for supply signals now need to be

    realized using signal polygons.

     

      - When a board drawing from an older version of EAGLE is loaded, any

    supply layers it contains will be renamed by moving the '$' to the end

    of the name. This makes sure automated scripts that treat a supply layer

    as "negative" don't make a mistake, while still indicating that layer as

    having been a supply layer. The functionality of the supply layer is

    replaced by a signal polygon with the proper name, using the minimum

    wire width from the net class of that signal. The polygon is drawn into

    the former supply layer as a rectangular shape, covering the area

    defined by any wires in the Dimension layer, by pads or by vias. The

    Autorouter setup is modified in such a way that the layer containing the

    generated polygon is activated (with preferred direction '*'), and the

    costs for that layer set to 99 in all passes.

     

    VERY IMPORTANT:

     

    After updating a board with supply layers from an older version, make

    sure you run the RATSNEST command to verify whether all pads are still

    connected to the respective signal.

     

     

    HTH

    Warren

    --

    ... use NNTP://news.cadsoft.de and a functional news reader like

    Thunderbird!

    ... or http://www.eaglecentral.ca browser access to CadSoft EAGLE

    support forums.

     

    ---

    This email has been checked for viruses by Avast antivirus software.

    https://www.avast.com/antivirus

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to SMD111

    On 22/07/2017 8:14 a.m., SMD111 wrote:

    Hi Warren, thank you for replying.

     

    I have EAGLE 6.4.0 Professional. It is old, but I like "good old" things image

     

    And for copying, I just select the copy mode on the toolbar, then click on the gate, then the IC is duplicated and stuck to cursor, then I place it with a click. After that I press "Switch to board" button and see airwires in some places where traces used to be.

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/225833

     

     

    The problem could be the following if the board is from a version prior

    to v6.

     

    The following is copied from the release notes (UPDATE_en.txt) which

    comes with Eagle.

     

    • Supply layers:

     

      - Supply layers (i.e. layers with names that start with a '$') are no

    longer treated special. Layers for supply signals now need to be

    realized using signal polygons.

     

      - When a board drawing from an older version of EAGLE is loaded, any

    supply layers it contains will be renamed by moving the '$' to the end

    of the name. This makes sure automated scripts that treat a supply layer

    as "negative" don't make a mistake, while still indicating that layer as

    having been a supply layer. The functionality of the supply layer is

    replaced by a signal polygon with the proper name, using the minimum

    wire width from the net class of that signal. The polygon is drawn into

    the former supply layer as a rectangular shape, covering the area

    defined by any wires in the Dimension layer, by pads or by vias. The

    Autorouter setup is modified in such a way that the layer containing the

    generated polygon is activated (with preferred direction '*'), and the

    costs for that layer set to 99 in all passes.

     

    VERY IMPORTANT:

     

    After updating a board with supply layers from an older version, make

    sure you run the RATSNEST command to verify whether all pads are still

    connected to the respective signal.

     

     

    HTH

    Warren

    --

    ... use NNTP://news.cadsoft.de and a functional news reader like

    Thunderbird!

    ... or http://www.eaglecentral.ca browser access to CadSoft EAGLE

    support forums.

     

    ---

    This email has been checked for viruses by Avast antivirus software.

    https://www.avast.com/antivirus