Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Unexpected behavior of EAGLE layout editor
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 16 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 3134 views
  • Users 0 members are here
  • eagle 6.4.0 professional
  • Layout Editor
Related

Unexpected behavior of EAGLE layout editor

SMD111
SMD111 over 9 years ago

The problem I have is described in the attached images (they are zoom-able).

I have a finalized, fully routed design:

image

At some point I decided to add a new gate to the schematic, so I copy IC5 and paste it as IC9. Please note that no connections on IC9 have been made yet:

image

Simply placing this gate on schematic causes significant changes on the board. As you can see, multiple nets become ripped up, even the nets that have nothing to do with IC5 or IC9.

image

Is it possible to avoid this effect?

Thank you,

Sergey

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 9 years ago

    On 21/07/17 16:35, SMD111 wrote:

    The problem I have is described in the attached images (they are zoom-able).

    I have a finalized, fully routed design:

     

    In what sense is that "fully routed"? The tiny schematic fragment

    clearly shows C5 connected to the power pins of two ICs but on that

    board it's only connected to a jumper. It's blatantly not complete.

     

    At some point I decided to add a new gate to the schematic, so I copy IC5 and paste it as IC9. Please note that no connections on IC9 have been made yet:

    Simply placing this gate on schematic causes significant changes on the board. As you can see, multiple nets become ripped up, even the nets that have nothing to do with IC5 or IC9.

     

    No changes to the board, no nets ripped up, merely the airwires have

    been turned on.

     

    Is it possible to avoid this effect?

     

    Yes, by starting with an actually completely routed board.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • SMD111
    0 SMD111 over 9 years ago in reply to autodeskguest

    No thanks for "blatantly" obnoxious response, but I owe you a reply.

     

    In what sense is that "fully routed"?

    In that sense that is shown on the first picture. This board has been in production for years.

     

     

    The tiny schematic fragment

    Oh, would you want to see the entire schematic? Bummer, it is proprietary!

     

    clearly shows C5 connected to the power pins of two ICs but on that

    board it's only connected to a jumper. It's blatantly not complete.

    C5 is connected to inner power supply layers, FYI.

     

    No changes to the board, no nets ripped up, merely the airwires have been turned on.

    The rip up procedure converts a routed trace to an airwire.

    If you can't see the difference between the first and the second board pictures, please don't bother polluting this forum.

     

    Yes, by starting with an actually completely routed board.

    It looks like you are also unfamiliar with the term "routing"

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to SMD111

    On 21/07/17 19:31, SMD111 wrote:

    No thanks for "blatantly" obnoxious response, but I owe you a reply.

     

    Merely pointing out what I see. It's only obnoxious if you choose to be

    offended by the truth.

     

    In what sense is that "fully routed"?

    In that sense that is shown on the first picture. This board has been in production for years.

    ++

     

    As I said, the image clearly shows it's not routed. It may well have

    been in production for years but not from that layout if it ever worked.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • SMD111
    0 SMD111 over 9 years ago in reply to autodeskguest

    "As I said, the image clearly shows it's not routed. It may well have

    been in production for years but not from that layout if it ever worked."

     

    This discussion is going nowhere. Let us stop this nonsense.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • SMD111
    0 SMD111 over 9 years ago in reply to autodeskguest

    "As I said, the image clearly shows it's not routed. It may well have

    been in production for years but not from that layout if it ever worked."

     

    This discussion is going nowhere. Let us stop this nonsense.