Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Through Hole Components Question
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 187 subscribers
  • Views 1292 views
  • Users 0 members are here
Related

Through Hole Components Question

ggates31
ggates31 over 9 years ago

I'm new to Eagle and was looking for some help with making a PCB board layout that I will have fabricated by a board manufacturer. The goal for my project that I'm working on was to have several capacitors and resistors connected with traces to two different through-hole components, a 12x2 pin female connector (something like this: https://www.digikey.com/product-detail/en/sullins-connector-solutions/PPPC122LFBN-RC/S7115-ND/810251.)

and a right angle 3 pin connector (something like this: https://www.digikey.com/product-detail/en/sullins-connector-solutions/PPTC031LGBN-RC/S5439-ND/775897)

I'd like to have the pins of the connectors soldered to through holes where they connect to the traces on the top layer (ideally the only layer) of the board. The plastic of the 12x2 connector should be positioned below the top layer with the pins facing upwards, and the plastic piece of the 3 pin connector should be above the top layer of the board. I've attached a couple pictures of how I have it currently designed in my Eagle board layout.

 

As for my actual questions:

As it is now, I don't have any through holes that I individually placed on the board, just the through-hole components themselves, so if I sent it to a manufacturer, how would it be printed? Do I need to add another layer to the board and through-holes in order to specify more accurately how I want the board to be made, and if so, how would I do this?

 

Thanks in advance!

 

imageimage

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 9 years ago

    Am 16.08.2017 um 20:03 schrieb Gary Gates:

    I'm new to Eagle and was looking for some help with making a PCB board layout that I will have fabricated by a board manufacturer. The goal for my project that I'm working on was to have several capacitors and resistors connected with traces to two different through-hole components, a 12x2 pin female connector (something like this: https://www.digikey.com/product-detail/en/sullins-connector-solutions/PPPC122LFBN-RC/S7115-ND/810251.)

    and a right angle 3 pin connector (something like this: https://www.digikey.com/product-detail/en/sullins-connector-solutions/PPTC031LGBN-RC/S5439-ND/775897)

    I'd like to have the pins of the connectors soldered to through holes where they connect to the traces on the top layer (ideally the only layer) of the board. The plastic of the 12x2 connector should be positioned below the top layer with the pins facing upwards, and the plastic piece of the 3 pin connector should be above the top layer of the board. I've attached a couple pictures of how I have it currently designed in my Eagle board layout.

     

    As for my actual questions:

    As it is now, I don't have any through holes that I individually placed on the board, just the through-hole components themselves, so if I sent it to a manufacturer, how would it be printed? Do I need to add another layer to the board and through-holes in order to specify more accurately how I want the board to be made, and if so, how would I do this?

     

    Thanks in advance!

     

      

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/227267

     

     

    VIAs.  Just place vias in your desired drill / diameter / shape.

    Remember to give them the name of the net they belong to (VIA

    'netname').  Then they become part of the net and get an airwire you can

    route.

     

    VIAs do not appear in the schematic and the don't get NAMEs or VALUES in

    the place plan.

    If you want solder pads to connect external wires, you want to see them

    in the schematic and in the place plan.  In that case you need a

    complete device you place in the schematic.  See wirepad.lbr,

    solpad.lbr, holes.lbr, testpad.lbr for examples.

     

     

    HTH, Hans

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 9 years ago

    Am 16.08.2017 um 20:03 schrieb Gary Gates:

    I'm new to Eagle and was looking for some help with making a PCB board layout that I will have fabricated by a board manufacturer. The goal for my project that I'm working on was to have several capacitors and resistors connected with traces to two different through-hole components, a 12x2 pin female connector (something like this: https://www.digikey.com/product-detail/en/sullins-connector-solutions/PPPC122LFBN-RC/S7115-ND/810251.)

    and a right angle 3 pin connector (something like this: https://www.digikey.com/product-detail/en/sullins-connector-solutions/PPTC031LGBN-RC/S5439-ND/775897)

    I'd like to have the pins of the connectors soldered to through holes where they connect to the traces on the top layer (ideally the only layer) of the board. The plastic of the 12x2 connector should be positioned below the top layer with the pins facing upwards, and the plastic piece of the 3 pin connector should be above the top layer of the board. I've attached a couple pictures of how I have it currently designed in my Eagle board layout.

     

    As for my actual questions:

    As it is now, I don't have any through holes that I individually placed on the board, just the through-hole components themselves, so if I sent it to a manufacturer, how would it be printed? Do I need to add another layer to the board and through-holes in order to specify more accurately how I want the board to be made, and if so, how would I do this?

     

    Thanks in advance!

     

      

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/227267

     

     

    VIAs.  Just place vias in your desired drill / diameter / shape.

    Remember to give them the name of the net they belong to (VIA

    'netname').  Then they become part of the net and get an airwire you can

    route.

     

    VIAs do not appear in the schematic and the don't get NAMEs or VALUES in

    the place plan.

    If you want solder pads to connect external wires, you want to see them

    in the schematic and in the place plan.  In that case you need a

    complete device you place in the schematic.  See wirepad.lbr,

    solpad.lbr, holes.lbr, testpad.lbr for examples.

     

     

    HTH, Hans