EAGLE User Support (English) Eagle 8.5.1 Air Wire Errors
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
  • State Verified Answer
  • Replies 11 replies
  • Answers 2 answers
  • Subscribers 182 subscribers
  • Views 4801 views
  • Users 0 members are here
Related

Eagle 8.5.1 Air Wire Errors

rarndt
rarndt over 8 years ago

With Eagle 8.5.1 I have air wire errors that I can not figure out how to correct (see attached).  I am modifying a PWB created in previous Eagle version, by adding one tri-color LED.  Both pins 1 (Din) and 2 (VCC) of the LED show air wires, and it is so small that I can't zoom in to see it.  Pin 3 (GND) routes fine to the GND polygon.  I have tried re-routing these two lines many times, with exact same results.  This LED is the only thing I have added to this board using Eagle 8.5.1.  Guidance please.

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • autodeskguest
    autodeskguest over 8 years ago in reply to dukepro +1
    Am 02.01.2018 um 23:26 schrieb Chuck Huber: On 01/02/2018 10:13 AM, rachaelp wrote: Hi Chuck, in EAGLE v8 (not sure the specific version it became available), you don't need that catch factor trick anymore…
  • dukepro
    dukepro over 8 years ago in reply to rachaelp +1
    On 01/02/2018 06:06 PM, rachaelp wrote: wrote: I guess it's time for me to retire from the news groups into reclusion, where the only company I have is v7. No!!!! Still lots of v7 and earlier users and…
  • autodeskguest
    0 autodeskguest over 8 years ago

    On 31/12/2017 4:28 a.m., Richard Arndt wrote:

    With Eagle 8.5.1 I have air wire errors that I can not figure out how to correct (see attached).  I am modifying a PWB create in previous Eagle version, by adding one tri-color LED.  Both pins 1 (Din) and 2 (VCC) of the LED show air wires, and it is so small that I can't zoom in to see it.  Pin 3 (GND) routes fine to the GND polygon.  I have tried re-routing these two lines many times, with exact same results.  Guidance please.

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/232872

     

    Attachments:

    airwire.PNG

     

     

    Hi Richard

     

    I suggest that you open the schematic and move the led and observe if

    the nets remain attached to the pins. Doing this could show up nets that

    are not connected to the pins. If that looks OK, next run a ERC check to

    see if that reveals any clues. Not likely as airwires seem to be present

    and so Eagle believes an airwire is justified between two points.

     

     

    Next, back on the board, move the LED ( you may care to record its XY

    location so you can return it to the current location later.

     

    When the led is moved do the routed traces at the pins move with the

    led? If not another question arises, did you use the ROUTE command to

    add the traces  which will snap to pads and airwire ends or use the WIRE

    command which wont snap to airwire ends and so you can be left with tiny

    airwires?

     

    With the LED moved, run the DRC, Hope fully the airwires may be larger

    now and then you will be able to get INFORMATION (net name) from them.

     

    Then I would try to pick them up with a route command. CliCk ROUTE and

    then click on the end of the airwire. Then drag out a route to somewhere

    convenient so you can then learn something about the signal name of the

    airwire.

     

    I assume this is a double sided board. Check you have the layers defined

    correctly in the DRC.

     

    Questions: Is the schematic and Board consistent?

     

    HTH

    Warren

     

     

     

    --

    ... use NNTP://news.cadsoft.de and a functional news reader like

    Thunderbird!

     

    ---

    This email has been checked for viruses by Avast antivirus software.

    https://www.avast.com/antivirus

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dukepro
    0 dukepro over 8 years ago

    On 12/30/2017 10:28 AM, Richard Arndt wrote:

    With Eagle 8.5.1 I have air wire errors that I can not figure out how to correct (see attached).  I am modifying a PWB create in previous Eagle version, by adding one tri-color LED.  Both pins 1 (Din) and 2 (VCC) of the LED show air wires, and it is so small that I can't zoom in to see it.  Pin 3 (GND) routes fine to the GND polygon.  I have tried re-routing these two lines many times, with exact same results.  Guidance please.

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/232872

     

    Attachments:

    airwire.PNG

     

     

    Richard,

     

    From the board layout editor, go to Options -> Set -> Misc and set the

    Catch factor to 0.

     

    Then, start a route (Edit -> Route), and click anywhere in the layout

    editor.  The nearest air wire will start to route.  Move the cursor

    around and zoom in and out to locate the air wire.

     

    By setting the catch factor to zero, the Route function will pick the

    nearest air wire without limitations on how far that air wire is from

    the click location.

     

    Hope this helps,

     

    - Chuck

     

    Attachments:
    8585.att1.html.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • rachaelp
    0 rachaelp over 8 years ago

    Hi Richard, This was reported on the main Autodesk EAGLE forums just before Christmas. They've identified the cause now I believe and it'll be fixed ASAP.

     

    Hi Chuck, in EAGLE v8 (not sure the specific version it became available), you don't need that catch factor trick anymore as airwires have a section in DRC so you can find them easily by clicking on them in there.

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dukepro
    0 dukepro over 8 years ago in reply to rachaelp

    On 01/02/2018 10:13 AM, rachaelp wrote:

    Hi Chuck, in EAGLE v8 (not sure the specific version it became available), you don't need that catch factor trick anymore as airwires have a section in DRC so you can find them easily by clicking on them in there.

     

    Well, THAT's an improvement.  I've manufactured at least one design that

    still had an air wire.  I hope the didn't remove existing functionality.

     

    I guess it's time for me to retire from the news groups into reclusion,

    where the only company I have is v7.

     

    Sayonara,

        - Chuck

     

     

    Attachments:
    1651.att1.html.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 8 years ago in reply to dukepro

    Hi Chuck,

    dukepro  wrote:

     

    Well, THAT's an improvement.  I've manufactured at least one design that still had an air wire.  I hope they didn't remove existing functionality.

    Nope, the existing functionality is still there :-)

    dukepro  wrote:

     

    I guess it's time for me to retire from the news groups into reclusion, where the only company I have is v7.

    No!!!! Still lots of v7 and earlier users and a lot of your expertise is still very relevant for v8 issues! Definitely not anywhere near time for you to retire from here image

     

    You should give a recent freeware version of v8 a try if you haven't already. They now have Push&Shove and also integrated SPICE simulation. It's improving a lot.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 8 years ago in reply to dukepro

    Am 02.01.2018 um 23:26 schrieb Chuck Huber:

    On 01/02/2018 10:13 AM, rachaelp wrote:

    Hi Chuck, in EAGLE v8 (not sure the specific version it became available), you don't need that catch factor trick anymore as airwires have a section in DRC so you can find them easily by clicking on them in there.

     

    Well, THAT's an improvement.  I've manufactured at least one design that

    still had an air wire.  I hope the didn't remove existing functionality.

     

    I guess it's time for me to retire from the news groups into reclusion,

    where the only company I have is v7.

     

    Sayonara,

        - Chuck

     

     

    Hi Chuck I am on V6 and stay there.

    Stay here your valuable advices are always welcome.

     

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dukepro
    0 dukepro over 8 years ago in reply to rachaelp

    On 01/02/2018 06:06 PM, rachaelp wrote:

      wrote:

    I guess it's time for me to retire from the news groups into reclusion, where the only company I have is v7.

    No!!!! Still lots of v7 and earlier users and a lot of your expertise is still very relevant for v8 issues! Definitely not anywhere near time for you to retire from here image

     

    You should give a recent freeware version of v8 a try if you haven't already. They now have Push&Shove and also integrated SPICE simulation. It's improving a lot.

     

    Sounds nice.  However, until they provide a perpetual license, and time

    I spend exploring v8 is a waste.  Much of the work I do is on a secured

    network, and I can't be plugging machines into the Internet just so that

    Eagle can phone home - whether it's once every 14 days, or once a year. 

    Can't do it.

     

    I expressed to Jorge some time ago my position.  Many of the new

    features in v8 are very attractive to me, and I would love to explore

    them.  But until the licensing issue is fixed to our satisfaction, it's

    pointless.  Right now, I think that Autodesk will never provide this

    option, which means that when the time comes that our needs dictate more

    functionality than what v7 has to offer, I will have to exclude v8 from

    the qualification process.

     

    'nuf of that whiney license stuff.

     

    As far as hanging around, I'll continue to monitor the newsgroups until

    Autodesk retires them.  Since they would rather steer their users to the

    web with all the non-Autodesk crap that gets loaded, the NNTP servers

    probably won't be around much longer.

     

    What a bleak outlook.  This sucks, doesn't it?

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rarndt
    0 rarndt over 8 years ago in reply to dukepro

    Yes, this did correct the problem.  It does make group move not work, since then grouping selects the nearest component rather than allowing you to select a group of components.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rarndt
    0 rarndt over 8 years ago in reply to rachaelp

    Thank you...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 8 years ago

    As a follow up, Autodesk have released a bug fix release 8.5.2 which can be found here.

     

    This release fixes the known airwire issue and also an issue with incorrectly highlighting nets and showing them on other pages when adding to an existing net.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>