Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) How to auto-route in only .brd file
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 3 answers
  • Subscribers 190 subscribers
  • Views 1714 views
  • Users 0 members are here
  • vias and traces
  • brd file
  • eagle autorouter
Related

How to auto-route in only .brd file

kishan07
kishan07 over 8 years ago

I have a .brd file with 100 pairs of through-hole vias (see the green vias in attached image). Each pair is supposed to be used as power and ground for micro-devices.

 

The via's outer diameter is .5 mm and the actual via hole is .15 mm. Since it is quite difficult to solder to such small vias to wires, I was thinking about routing traces from vias to pads for pin headers at the edge of the board.

 

The problem is since this is a .brd file (no schematic) and there is no other components except vias I cannot use the autoroute function. Is there a way to auto-route the traces from vias to pads for external header connectors?

 

image

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 8 years ago

    On 4/01/2018 12:57 p.m., Tanvir Ahmad wrote:

    I have a .brd file with 100 pairs of through-hole vias (see the green vias in attached image). Each pair is supposed to be used as power and ground for micro-devices.

     

    The via's outer diameter is .5 mm and the actual via hole is .15 mm. Since it is quite difficult to solder to such small vias to wires, I was thinking about routing traces from vias to pads for pin headers at the edge of the board.

     

    The problem is since this is a .brd fle and there is no other components except vias I cannot use the autoroute function. Is there a way to auto-route the traces from vias to pads for external header connectors?

     

     

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/233016

     

     

     

    Hi

    I suspect your approach may not be the best.

     

    A few questions:

    Does there have to be a trace out to the header pin for every via?

    That's 200 header pins. Or if they are power and ground can all the

    grounds and power vias be connected and a single trace taken to a 2 pin

    header?

     

    Do your micro devices have wires that fit through the 0.15mm holes?

    Perhaps they are surface mount devices.

     

    Even when working with just the board it is usually preferable to use

    packages from a library. That would give you a pad or smd to run a

    signal between on the board an then the auto router will work.

     

    Let us know

    Warren

     

    --

    ... use NNTP://news.cadsoft.de and a functional news reader like

    Thunderbird!

     

    ---

    This email has been checked for viruses by Avast antivirus software.

    https://www.avast.com/antivirus

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 8 years ago

    On 4/01/2018 12:57 p.m., Tanvir Ahmad wrote:

    I have a .brd file with 100 pairs of through-hole vias (see the green vias in attached image). Each pair is supposed to be used as power and ground for micro-devices.

     

    The via's outer diameter is .5 mm and the actual via hole is .15 mm. Since it is quite difficult to solder to such small vias to wires, I was thinking about routing traces from vias to pads for pin headers at the edge of the board.

     

    The problem is since this is a .brd fle and there is no other components except vias I cannot use the autoroute function. Is there a way to auto-route the traces from vias to pads for external header connectors?

     

     

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/233016

     

     

     

    Hi

    I suspect your approach may not be the best.

     

    A few questions:

    Does there have to be a trace out to the header pin for every via?

    That's 200 header pins. Or if they are power and ground can all the

    grounds and power vias be connected and a single trace taken to a 2 pin

    header?

     

    Do your micro devices have wires that fit through the 0.15mm holes?

    Perhaps they are surface mount devices.

     

    Even when working with just the board it is usually preferable to use

    packages from a library. That would give you a pad or smd to run a

    signal between on the board an then the auto router will work.

     

    Let us know

    Warren

     

    --

    ... use NNTP://news.cadsoft.de and a functional news reader like

    Thunderbird!

     

    ---

    This email has been checked for viruses by Avast antivirus software.

    https://www.avast.com/antivirus

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • kishan07
    0 kishan07 over 8 years ago in reply to autodeskguest

    Hi Warren,

    Thanks for your feedback.

    These microdevices are two terminal devices which need to be powered separately. I can try to tie all the grounds together into one pin, but I still need 100 power pins for independent operations of the microdevices.