Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) How to auto-route in only .brd file
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 3 answers
  • Subscribers 190 subscribers
  • Views 1710 views
  • Users 0 members are here
  • vias and traces
  • brd file
  • eagle autorouter
Related

How to auto-route in only .brd file

kishan07
kishan07 over 8 years ago

I have a .brd file with 100 pairs of through-hole vias (see the green vias in attached image). Each pair is supposed to be used as power and ground for micro-devices.

 

The via's outer diameter is .5 mm and the actual via hole is .15 mm. Since it is quite difficult to solder to such small vias to wires, I was thinking about routing traces from vias to pads for pin headers at the edge of the board.

 

The problem is since this is a .brd file (no schematic) and there is no other components except vias I cannot use the autoroute function. Is there a way to auto-route the traces from vias to pads for external header connectors?

 

image

  • Sign in to reply
  • Cancel
Parents
  • elliiot14
    0 elliiot14 over 8 years ago

    Eagle must know the signal name of connected vias.

     

    Name them, after there are unrouted "ribbons" between equal named vias (Layer 19).

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • elliiot14
    0 elliiot14 over 8 years ago

    Eagle must know the signal name of connected vias.

     

    Name them, after there are unrouted "ribbons" between equal named vias (Layer 19).

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • autodeskguest
    0 autodeskguest over 8 years ago in reply to elliiot14

    On 4/01/2018 9:32 p.m., J. Martens wrote:

    Eagle must know the signal name of connected vias.

     

    So give them one and you see the connection as ribbon on layer 19 tha can be routed.

     

     

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/233082

     

     

     

    When there is only the board, the above does not achieve the

    airwires/nets/signals. Rememeber there is no schematic and hence there

    are no known nets or connections.

     

    When creating the SIGNAL it cannot be connected to the via but if the

    signal is created first and then you name the via, it will pick up an

    airwire.

     

    The problem is, the OP talks of a header where one pad of which connects

    to the via. To get the signal in the first place, the header pad needs

    to connect to another pad or SMD. It cannot be established to a named

    via. Once you have a signal between two pads, you can view the name of

    the signal on the header pad and then name the respective via and an

    airwire will appear. Then you can delete the unwanted airwire and the

    other package that was used to get a pad temporarily for the first step.

     

    HTH

    Warren

     

     

     

    --

    ... use NNTP://news.cadsoft.de and a functional news reader like

    Thunderbird!

     

    ---

    This email has been checked for viruses by Avast antivirus software.

    https://www.avast.com/antivirus

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer