Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Move Part / Device to Other Layer (Bottom)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 5577 views
  • Users 0 members are here
Related

Move Part / Device to Other Layer (Bottom)

phased
phased over 8 years ago

Hello,

 

I have been working on a PCB design which is intended to use an edge card connector. I first created a package / symbol / device which represented this connector as having copper (fingers) on both the top and bottom layers. However, when attempting to export the routing files to a manufacturing house, I got a failure message with errors such as: Your project doesn't contain a bottom copper file and Your project doesn't contain a bottom solder mask.

So this made me realize that, even though I created the package to have copper on both Top and Bottom layers, the board layout kept both sets of copper on the Top layer.

 

After this, I attempted to create a device which had only one set of fingers so I could put device on the Top layer and another on the Bottom layer. However, apparently Eagle will not allow me to put a device on the Bottom layer.

 

Can anyone tell me if there is something special I need to do to accomplish this or if I am going about the process of adding edge connector fingers to a board incorrectly and how I may do it differently?

 

Thank you very much in advance!

 

Troy.

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 8 years ago

    Am 22.03.2018 um 17:30 schrieb Troy Whipple:

    Hello,

     

    I have been working on a PCB design which is intended to use an edge card connector. I first created a package / symbol / device which represented this connector as having copper (fingers) on both the top and bottom layers. However, when attempting to export the routing files to a manufacturing house, I got a failure message with errors such as: Your project doesn't contain a bottom copper file and Your project doesn't contain a bottom solder mask.

    So this made me realize that, even though I created the package to have copper on both Top and Bottom layers, the board layout kept both sets of copper on the Top layer.

     

    After this, I attempted to create a device which had only one set of fingers so I could put device on the Top layer and another on the Bottom layer. However, apparently Eagle will not allow me to put a device on the Bottom layer.

     

    Can anyone tell me if there is something special I need to do to accomplish this or if I am going about the process of adding edge connector fingers to a board incorrectly and how I may do it differently?

     

    Thank you very much in advance!

     

    Troy.

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/237262

     

     

    Hi,

    use the "Mirror" command to put a device from

    top-layer to bottom-layer(or back)

    This will switch the layers of the device

    1,21,23,25,27,29,31,33,35,37,39,41 to

    2,22,24,26,28,30,32,34,36,38,40,42

     

    HTH

    Werner

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • phased
    0 phased over 8 years ago in reply to autodeskguest

    Hello Werner,

     

    Thanks for your reply! Unfortunately, when I attempt to use the mirror function on this, Eagle does not recognize the device as an object it can mirror. Eagle does recognize the device when I use the move function so I find this strange.

    Of course, I have attempted to move the device to another layer but that does not work. I am open to any suggestions.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 8 years ago in reply to phased

    Am 23.03.2018 um 13:52 schrieb Troy Whipple:

    Hello Werner,

     

    Thanks for your reply! Unfortunately, when I attempt to use the mirror function on this, Eagle does not recognize the device as an object it can mirror. Eagle does recognize the device when I use the move function so I find this strange.

    Of course, I have attempted to move the device to another layer but that does not work. I am open to any suggestions.

     

    Hello Troy,

    some Questions:

    Eagle Versiom?

    Can you try a "mirror" on an other device on the Board?

    Its only for testing to look is the issue in eagle or the device.

     

    Werner

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 8 years ago in reply to phased

    Am 23.03.2018 um 13:52 schrieb Troy Whipple:

    Hello Werner,

     

    Thanks for your reply! Unfortunately, when I attempt to use the mirror function on this, Eagle does not recognize the device as an object it can mirror. Eagle does recognize the device when I use the move function so I find this strange.

    Of course, I have attempted to move the device to another layer but that does not work. I am open to any suggestions.

     

    Hello Troy,

    some Questions:

    Eagle Versiom?

    Can you try a "mirror" on an other device on the Board?

    Its only for testing to look is the issue in eagle or the device.

     

    Werner