Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) DXF export content question
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 187 subscribers
  • Views 963 views
  • Users 0 members are here
  • dxf
Related

DXF export content question

rht
rht over 8 years ago

Is it possible to export a DXF of the copper traces with the component holes shown so that a home etched test board will have all the holes located after etching?

I'm used to laying out my PC board using ACAD which, when completed, has all the holes for components showing (typically 0.020" dia.) so the centers are etched ready for drilling.

I can export the copper DXF from Eagle to my ACAD for the test board transparency but no hole centers show to etch for drill location. Perhaps this is not something you can do using Eagle? I do like many of the other features of the program, but would still like to use it to make my test PCB before shipping out for professional manufacture! Any thoughts would be appreciated.

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 8 years ago

    On 06/05/18 19:13, Russel Tully wrote:

    Is it possible to export a DXF of the copper traces with the component holes shown so that a home etched test board will have all the holes located after etching?

    I'm used to laying out my PC board using ACAD which, when completed, has all the holes for components showing (typically 0.020" dia.) so the centers are etched ready for drilling.

    I can export the copper DXF from Eagle to my ACAD for the test board transparency but no hole centers show to etch for drill location. Perhaps this is not something you can do using Eagle? I do like many of the other features of the program, but would still like to use it to make my test PCB before shipping out for professional manufacture! Any thoughts would be appreciated.

     

    When I've done home-etch transparencies I've always used the print

    functions, which leave a hole in the pad. There's a ULP that puts an

    extra ring on a documentation layer to give you the small pilot hole you

    want.

     

    I'm not sure how you'd get that with DXF but you definitely need to

    export more than just the copper layer (16) as the holes are not part of

    the copper.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 8 years ago

    On 06/05/18 19:13, Russel Tully wrote:

    Is it possible to export a DXF of the copper traces with the component holes shown so that a home etched test board will have all the holes located after etching?

    I'm used to laying out my PC board using ACAD which, when completed, has all the holes for components showing (typically 0.020" dia.) so the centers are etched ready for drilling.

    I can export the copper DXF from Eagle to my ACAD for the test board transparency but no hole centers show to etch for drill location. Perhaps this is not something you can do using Eagle? I do like many of the other features of the program, but would still like to use it to make my test PCB before shipping out for professional manufacture! Any thoughts would be appreciated.

     

    When I've done home-etch transparencies I've always used the print

    functions, which leave a hole in the pad. There's a ULP that puts an

    extra ring on a documentation layer to give you the small pilot hole you

    want.

     

    I'm not sure how you'd get that with DXF but you definitely need to

    export more than just the copper layer (16) as the holes are not part of

    the copper.