Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Two components behave like one
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 727 views
  • Users 0 members are here
Related

Two components behave like one

jan89
jan89 over 8 years ago

Hello,

 

I created a schematic in Eagle using 6 pairs of PCIE slots (12 PCIE slots total). After neting them together and creating a board file from the schematic I discovered that each pair of the PCIE slots is treated in the board layout as one (I see only 6 slots in the board editor and they have doubled routes connected to them). When I try to rename one of the shots the second one from the pair gets the same name attached immediately. This messes the routing in the bord editor up. How can I rename the slots so that every single one will be treated individually and not as a pair?

 

Jan

  • Sign in to reply
  • Cancel
Parents
  • rachaelp
    0 rachaelp over 8 years ago

    Hi Jan,

     

    I suspect the PCIE connector library part you are using has the connector defined such that it has two symbols per connector, i.e. one symbol per each side of the connector. When you place 12 connector symbols in your board you are in fact placing the two halves of 6 connectors. You will be able to tell this because pairs of symbols will have matching reference designators, maybe something like J1A, J1B, J2A, J2B, etc. So you've got half the connectors you think you have.

     

    Now, it could be a case that the reason this has happened is due to the way the symbol is drawn making it look like it should be a single symbol per part so thoroughly check the library part you've used. As Warren says, the easiest way for us to give you a definitive answer is to zip up your scb/brd files and share them here.

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • rachaelp
    0 rachaelp over 8 years ago

    Hi Jan,

     

    I suspect the PCIE connector library part you are using has the connector defined such that it has two symbols per connector, i.e. one symbol per each side of the connector. When you place 12 connector symbols in your board you are in fact placing the two halves of 6 connectors. You will be able to tell this because pairs of symbols will have matching reference designators, maybe something like J1A, J1B, J2A, J2B, etc. So you've got half the connectors you think you have.

     

    Now, it could be a case that the reason this has happened is due to the way the symbol is drawn making it look like it should be a single symbol per part so thoroughly check the library part you've used. As Warren says, the easiest way for us to give you a definitive answer is to zip up your scb/brd files and share them here.

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer