Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Kelvin connection in Eagle
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Answers 4 answers
  • Subscribers 189 subscribers
  • Views 4263 views
  • Users 0 members are here
  • eagle
  • kelvin_resistor
  • eagle_cad
  • custom pcb
Related

Kelvin connection in Eagle

jjvan
jjvan over 8 years ago

Hey everyone!

 

I'm still learning eagle, so some obvious things are still difficult for me to wrap my head around, but I'm learning!

 

I have a question regarding Kelvin connections in Eagle. I have a board I need to design that performs current sensing. It has 2 input jacks, 2 output bnc jacks (that go to a differential amplifier) and a shunt resistor to measure the voltage drop across. My supervisor has asked me to implement the following pad layout for the kelvin connection with this shunt resistor: https://www.bourns.com/docs/Product-Datasheets/css2h-2512.pdf

image

To do this the only approach I could come up with was to design a new footprint for the shunt resistor in which both sides have 3 pads. So I came up with this footprint (Bourns_CSS2H-2512-A in this library: https://github.com/joshvandermeer/Eaglelibrary )

 

image

Then when I try to connect to the pads manually using the polygon tool in eagle, I get the following:

image

Where it looks like each pad has a maximum trace width for the trace connecting to it. This circuit will have a high current, so I want the traces to connect completely, not just by a thin trace at the terminals.

 

Is there anything I can do to improve this situation? I'm new to this, so I'm sure I'm overlooking something important, and I really appreciate any advice!

 

Thank you!

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 7 years ago

    On 08.10.2018 17:06, Joshua Vandermeer wrote:

    Hey everyone!

     

    I'm still learning eagle, so some obvious things are still difficult for me to wrap my head around, but I'm learning!

     

    I think you are way overdoing this circuit, and at the same time you

    weaken it. If the resistor is tightly dimensioned for your power, you

    need the full pad both for heatsink and current.

     

    Just route the kelvin probes out on the side of the SMD pads. The point

    of the kelvin probes are to avoid the voltage drop in the high current

    main path. If you just bring out some probes on the side of the smd's,

    there will be close to no current generating voltage drop on those

    tracks. If you want max noise immunity, route the two tracks

    differential back to the sensing circuit. For even more noise immunity

    route them through directly down a VIA to a different opposite layer.

     

    The implementation of the kelvin probes is done at the board layouyt,

    not the schematic, but if you need others to do the routing job based on

    your schematic drawings, draw it like you would route it and put a

    comment in the schematic at the info or guide layer.

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rachaelp
    0 rachaelp over 7 years ago in reply to autodeskguest

    autodeskguest  wrote:

     

    I think you are way overdoing this circuit, and at the same time you

    weaken it. If the resistor is tightly dimensioned for your power, you

    need the full pad both for heatsink and current.

     

    Just route the kelvin probes out on the side of the SMD pads.

     

    Joshua does say in his first post "My supervisor has asked me to implement the following pad layout for the kelvin connection with this shunt resistor". It might not be what you would do, but it is what he was asked to implement by his supervisor.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 7 years ago in reply to rachaelp

    On 15.10.2018 11:01, rachaelp wrote:

      wrote:

     

    I think you are way overdoing this circuit, and at the same time you

    weaken it. If the resistor is tightly dimensioned for your power, you

    need the full pad both for heatsink and current.

     

    Just route the kelvin probes out on the side of the SMD pads.

     

    Joshua does say in his first post "My supervisor has asked me to implement the following pad layout for the kelvin connection with this shunt resistor". It might not be what you would do, but it is what he was asked to implement by his supervisor.

     

    Best Regards,

     

    Rachael

     

     

    Fair enough Rachael image

     

    If this was me, I would go back to my supervisor and demonstrate my

    skills and tell him about this implementations weakness but it may not

    be the right thing for Joshua this time. That's up to him.

     

    To add more feedback to his supervisor, Im not even sure if a

    manufacturer would like this implementation, due to it's potential

    bistable nature. When the lead melts, this got a bistable nature of not

    falling to rest on the large pads, but may be pulled to one side or the

    other.

     

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 7 years ago in reply to autodeskguest

    I had a similar need.

     

    What I ended up doing was to create a net class with special trace widths different from the rest on the board. THen When this is autorouted it always is routed directly to where it should be, nothing shared.

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/277798

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 7 years ago in reply to jjvan

    On 15.10.2018 17:19, Joshua Vandermeer wrote:

    Thank you both for the great advice. I agree that the implementation I was shooting for was very overcomplicated. I'm an intern right now and trying to take as much instruction as I can. I was given this document to follow, but there was a miscommunication and he just wanted me to learn from it, not actually implement it.

     

    Optimize High-Current Sensing Accuracy by Improving Pad Layout of Low-Value Shunt Resistors | Analog Devices (http://www.analog.com/en/analog-dialogue/articles/optimize-high-current-sensing-accuracy.html)

     

    Ended up just taking the kelvin connection from the inside of the pads.

     

    Interesting experiment there.. Using constant current source may not

    reveal all the weaknesses tho. Voltage applied to get to that current

    may vary to compensate higher R(solder) on the smaller area pads, and

    this may cause undesired effects. Also thermal effects may increase

    because of the same problem.

     

    Your conclusion seem to be something what I would do, but this is very

    dependant on how the resistor is actually built. Choosing the shortest

    path to the actual start of the resistor material would give best result.

     

    Because of the resistor physics, you could also analyze the result on

    different fine tuned positions of the resistor, but these are errors

    that are hard to control in mass production.

     

    If you really would need a high precision, high yield kelvin probe, some

    extra attention to all the side effects may be required, but usually you

    end up with some calibration process. This is why noise is more of a

    real problem than offset errors.

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jjvan
    0 jjvan over 7 years ago in reply to autodeskguest

    Thank you both for the great advice. I agree that the implementation I was shooting for was very overcomplicated. I'm an intern right now and trying to take as much instruction as I can. I was given this document to follow, but there was a miscommunication and he just wanted me to learn from it, not actually implement it.

     

    Optimize High-Current Sensing Accuracy by Improving Pad Layout of Low-Value Shunt Resistors | Analog Devices

     

    Ended up just taking the kelvin connection from the inside of the pads.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jjvan
    0 jjvan over 7 years ago in reply to autodeskguest

    Thank you both for the great advice. I agree that the implementation I was shooting for was very overcomplicated. I'm an intern right now and trying to take as much instruction as I can. I was given this document to follow, but there was a miscommunication and he just wanted me to learn from it, not actually implement it.

     

    Optimize High-Current Sensing Accuracy by Improving Pad Layout of Low-Value Shunt Resistors | Analog Devices

     

    Ended up just taking the kelvin connection from the inside of the pads.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • autodeskguest
    0 autodeskguest over 7 years ago in reply to autodeskguest

    I had a similar need.

     

    What I ended up doing was to create a net class with special trace widths different from the rest on the board. THen When this is autorouted it always is routed directly to where it should be, nothing shared.

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/277798

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 7 years ago in reply to jjvan

    On 15.10.2018 17:19, Joshua Vandermeer wrote:

    Thank you both for the great advice. I agree that the implementation I was shooting for was very overcomplicated. I'm an intern right now and trying to take as much instruction as I can. I was given this document to follow, but there was a miscommunication and he just wanted me to learn from it, not actually implement it.

     

    Optimize High-Current Sensing Accuracy by Improving Pad Layout of Low-Value Shunt Resistors | Analog Devices (http://www.analog.com/en/analog-dialogue/articles/optimize-high-current-sensing-accuracy.html)

     

    Ended up just taking the kelvin connection from the inside of the pads.

     

    Interesting experiment there.. Using constant current source may not

    reveal all the weaknesses tho. Voltage applied to get to that current

    may vary to compensate higher R(solder) on the smaller area pads, and

    this may cause undesired effects. Also thermal effects may increase

    because of the same problem.

     

    Your conclusion seem to be something what I would do, but this is very

    dependant on how the resistor is actually built. Choosing the shortest

    path to the actual start of the resistor material would give best result.

     

    Because of the resistor physics, you could also analyze the result on

    different fine tuned positions of the resistor, but these are errors

    that are hard to control in mass production.

     

    If you really would need a high precision, high yield kelvin probe, some

    extra attention to all the side effects may be required, but usually you

    end up with some calibration process. This is why noise is more of a

    real problem than offset errors.

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer