Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Adding libraries
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 178 subscribers
  • Views 328 views
  • Users 0 members are here
Related

Adding libraries

autodeskguest
autodeskguest over 17 years ago

When I open  one of my projects it loads all the libraries to the project.

Why is it doing that and how can I stop it? I only want the libraries I have

specifically added myself.

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    Richard_H over 17 years ago

    hcs schrieb:

    When I open  one of my projects it loads all the libraries to the project.

    Why is it doing that and how can I stop it? I only want the libraries I have

    specifically added myself.

     

     

     

     

    The USE command determins which libraries are shown with the ADD

    command. Best is to type in the command line, for example of the

    Schematic Editor:

     

      USE -*

     

    No library will be used. Now select the libnraries you want to

    see with ADD.

    This can be done in the Control Panel's tree view or with the

    Library/Use menu.

     

    The information which libraries are in use, is stored in the current

    eagle.epf file.

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 17 years ago

    hcs schrieb:

    When I open  one of my projects it loads all the libraries to the project.

    Why is it doing that and how can I stop it? I only want the libraries I have

    specifically added myself.

     

     

     

     

    The USE command determins which libraries are shown with the ADD

    command. Best is to type in the command line, for example of the

    Schematic Editor:

     

      USE -*

     

    No library will be used. Now select the libnraries you want to

    see with ADD.

    This can be done in the Control Panel's tree view or with the

    Library/Use menu.

     

    The information which libraries are in use, is stored in the current

    eagle.epf file.

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm