EAGLE User Support (English) Off-board question and a possible solution
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
  • Replies 2 replies
  • Subscribers 177 subscribers
  • Views 234 views
  • Users 0 members are here
Related

Off-board question and a possible solution

autodeskguest
autodeskguest over 17 years ago

I noticed today, after making my own library part for a 1/4" Mono Jack

Socket (Standard audio connector), and placing the pads quite a way

from the part outline on the Document layer (in the Package editor(?))

- that when I go to make a board, I can place the Pads of the

component on the edge of the Board as needed (where I'd solder leads

from the board to the Jack) without having the part outline actually

on the board.

 

This seems to let me use one Device on my Schematic and on my board

without having to make two schematics for on/off board components, or

use any of the other 'workarounds' that have been mentioned in the

group here.

 

I'm not getting any ERC or DRC errors in either the Board or Schematic

editors and don't need to worry about silk-screening or board-houses

as I'll be making my own boards.

 

Is there any reason why I shouldn't be doing this?

 

Any problems I'm likely to come up against when I come to make the

board?

 

Hope this all makes sense/helps. BTW I'm using the free/lite version

under X11 on a Mac - if that matters.

 

Many thanks for any input/advice on this.

 

--

I'm trying a new usenet client for Mac, Nemo OS X.

You can download it at http://www.malcom-mac.com/nemo

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    I have this issue all the time and I dont think there is a great workaround

    if you want connectivity for parts off the board that are hand wired.

     

    I use a separate Pad for connection on the board for instance tubes, I'll

    label them V1-1, V1-2 and you can use non metal layers to show connection on

    the board layout (but there is no connectivity) from the pad on the board to

    the offboard tube socket. You can create these off board items as symbols

    only with no pins.

     

    Not sure I understand about the pads on Document layer? They should be on

    the pad layer if they are on the board.

     

    New version is in beta but much better than the X11 version IMO, I prefer

    running Eagle on XP with the Mac Intel with Bootcamp until the Version 5 is

    all good to go.

     

    "J_ADT" <j_adt@email.com> wrote in message

    news:nemoTue012908082118@news.cadsoft.de...

    I noticed today, after making my own library part for a 1/4" Mono Jack

    Socket (Standard audio connector), and placing the pads quite a way

    from the part outline on the Document layer (in the Package editor(?))

    - that when I go to make a board, I can place the Pads of the

    component on the edge of the Board as needed (where I'd solder leads

    from the board to the Jack) without having the part outline actually

    on the board.

     

    This seems to let me use one Device on my Schematic and on my board

    without having to make two schematics for on/off board components, or

    use any of the other 'workarounds' that have been mentioned in the

    group here.

     

    I'm not getting any ERC or DRC errors in either the Board or Schematic

    editors and don't need to worry about silk-screening or board-houses

    as I'll be making my own boards.

     

    Is there any reason why I shouldn't be doing this?

     

    Any problems I'm likely to come up against when I come to make the

    board?

     

    Hope this all makes sense/helps. BTW I'm using the free/lite version

    under X11 on a Mac - if that matters.

     

    Many thanks for any input/advice on this.

     

    --

    I'm trying a new usenet client for Mac, Nemo OS X.

    You can download it at http://www.malcom-mac.com/nemo

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    I have this issue all the time and I dont think there is a great workaround

    if you want connectivity for parts off the board that are hand wired.

     

    I use a separate Pad for connection on the board for instance tubes, I'll

    label them V1-1, V1-2 and you can use non metal layers to show connection on

    the board layout (but there is no connectivity) from the pad on the board to

    the offboard tube socket. You can create these off board items as symbols

    only with no pins.

     

    Not sure I understand about the pads on Document layer? They should be on

    the pad layer if they are on the board.

     

    New version is in beta but much better than the X11 version IMO, I prefer

    running Eagle on XP with the Mac Intel with Bootcamp until the Version 5 is

    all good to go.

     

    "J_ADT" <j_adt@email.com> wrote in message

    news:nemoTue012908082118@news.cadsoft.de...

    I noticed today, after making my own library part for a 1/4" Mono Jack

    Socket (Standard audio connector), and placing the pads quite a way

    from the part outline on the Document layer (in the Package editor(?))

    - that when I go to make a board, I can place the Pads of the

    component on the edge of the Board as needed (where I'd solder leads

    from the board to the Jack) without having the part outline actually

    on the board.

     

    This seems to let me use one Device on my Schematic and on my board

    without having to make two schematics for on/off board components, or

    use any of the other 'workarounds' that have been mentioned in the

    group here.

     

    I'm not getting any ERC or DRC errors in either the Board or Schematic

    editors and don't need to worry about silk-screening or board-houses

    as I'll be making my own boards.

     

    Is there any reason why I shouldn't be doing this?

     

    Any problems I'm likely to come up against when I come to make the

    board?

     

    Hope this all makes sense/helps. BTW I'm using the free/lite version

    under X11 on a Mac - if that matters.

     

    Many thanks for any input/advice on this.

     

    --

    I'm trying a new usenet client for Mac, Nemo OS X.

    You can download it at http://www.malcom-mac.com/nemo

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • autodeskguest
    autodeskguest over 17 years ago in reply to autodeskguest

     

    I noticed today, after making my own library part for a 1/4" Mono

    Jack Socket (Standard audio connector), and placing the pads quite a

    way from the part outline on the Document layer (in the Package

    editor(?)) - that when I go to make a board, I can place the Pads of

    the component on the edge of the Board as needed (where I'd solder

    leads from the board to the Jack) without having the part outline

    actually on the board.

     

      This seems to let me use one Device on my Schematic and on my

    board without having to make two schematics for on/off board

    components, or use any of the other 'workarounds' that have been

    mentioned in the group here.

     

      I'm not getting any ERC or DRC errors in either the Board or

    Schematic editors and don't need to worry about silk-screening or

    board-houses as I'll be making my own boards.

     

      Is there any reason why I shouldn't be doing this?

     

      Any problems I'm likely to come up against when I come to make the

    board?

     

      Hope this all makes sense/helps. BTW I'm using the free/lite

    version under X11 on a Mac - if that matters.

     

      Many thanks for any input/advice on this.

     

    In article <fnthe0$9b1$1@cheetah.cadsoft.de> "John

    Suhr"<john@NOSPAMsuhrguitars.com> wrote:

    I have this issue all the time and I dont think there is a great

    workaround if you want connectivity for parts off the board that are

    hand wired.

     

    I use a separate Pad for connection on the board for instance tubes,

    I'll label them V1-1, V1-2 and you can use non metal layers to show

    connection on the board layout (but there is no connectivity) from

    the pad on the board to the offboard tube socket. You can create

    these off board items as symbols only with no pins.

     

    Not sure I understand about the pads on Document layer? They should

    be on the pad layer if they are on the board.

     

    New version is in beta but much better than the X11 version IMO, I

    prefer running Eagle on XP with the Mac Intel with Bootcamp until the

    Version 5 is all good to go.

     

    "J_ADT" <j_adt@email.com> wrote in message

    news:nemoTue012908082118@news.cadsoft.de...

     

    John,

     

    Thanks for this - you're solution is way better.

     

    J

     

     

    --

    I'm trying a new usenet client for Mac, Nemo OS X.

    You can download it at http://www.malcom-mac.com/nemo