"David Pollum" <vze24h5m@verizon.net> wrote in message
news:fm5iba$4pp$1@cheetah.cadsoft.de...
Ron wrote:
"Richard Hammerl" <ric@cadsoft.de> wrote in message
news:flsu6v$s66$1@cheetah.cadsoft.de...
<snip>
there seem to be lots of trouble with your board. Could you meanwhile
solve all the problems? If no, please send me the board file with
private mail so that I can check it.
--
Mit freundlichen Gruessen / Best regards
Richard Hammerl
CadSoft Support -- hotline@cadsoft.de
Offer much appreciated, but the "problem" is the newbie (me!) learning
curve. For example, it didn't really sink in until I came across a
message that I don't have to add a polygon in the Dimension layer, a line
will do along with proper Drc "Distance" settings. And the layer being
drawn on during routing, well, that too gets set in the "Route" section
of Drc. Via's occuring on power traces, well, I suspect it was just my
view of that board that used burried via's, turning off display layers I
don't think turns off seeing all burried via's on a turned off layer if
the display is set to show just 1 layer and via's; most houses seem to
give better deals if only via's that go through all layers are used
anyway. The Class thing works fine, but it was by pure curiosity that I
discovered that once I set Change|Class all I had to do was click a net
either in the schematic or the board editor and from thereon it would be
'remembered' in the project (needed for various size net widths). Now, I
don't think I really had 'overlaps' but instead was seeing all via's when
viewing just 1 layer, instead of just the via's that the layer has!
Ok, I know I sound stupid. I am! This is a difficult program to learn how
to use and too much documentation doesn't point back to things that one
really needs to already understand in order to then understand what is
being researched. But don't get me wrong, it's just a learning curve and
I am very impressed with how well Eagle works with or without quirks!
It's just that my 1st project, out of necessity and time constraints, had
to be a 4x5" board, 4 layers, with 31 IC's on it... it was "learn by
doing" because of that constraint on my time. But, I've done it, and I
understand a LOT more than I did just 2 weeks ago, and the gerber files
have even passed online testing.<grin>
I will, however, send ya copy of the project soon. I decreased the board
editor grid settings (have good reasons) and did some other improvements,
and so of course now it takes much longer (near 24 hours vs 6) to
autoroute but traces are closer (grid is finer, allowing Drc settings to
be effective). It's cooking at home now, on a darn fast computer, as I
write this just before I start work at my 'day job'...
-Ron
Ron;
That sounds like a pretty complicated board for a newbie to layout. Are
you just a newbie with EAGLE, or are you a PCB layout newbie, too? I'd be
interested in seeing the latest version of the board.
-Dave Pollum
My apology for the long response time.
Well, Dave and Richard, the answer is yes & yes. But decades away from being
a newbie to electronics itself. The breadboarded project circuit, and
software to use it, works. Regrettably, getting into board design is
something I should have gotten into at least a decade ago, as I find the
learning curve much steeper than anticipated. But ok, if I've made so much
noise that now 2 people have requested to see the board then I am grateful
and I'd like to comply. But I can not disclose the schematic. How do I go
about this, just send the 157k .brd file? Is it necessary to include any non
standard library I've created for the board, or anything else beyond just
the .brd file? Is it allowed to attach it to a reply to this ng topic even
though its 157k?
I'm still fighting 2 remaining battles.
freeDFM is complaining that all my vias have an annular ring (restring)
of 0mil, but my DRC table for vias looks identical to page 102 in the manual
(8mil/25%/20mil) and I changed the default class to read 6mil/6mil/15mil, so
I think at a drill of 15mil the ring is 16mil and not 0mil.
freeDFM is complaining that all text associated with all (yes, all)
packages is too small. I've no idea how to fix that without editing the
respective libraries, since smashing isn't the answer.
-Ron
I'm still fighting 2 remaining battles.
freeDFM is complaining that all my vias have an annular ring (restring)
of 0mil, but my DRC table for vias looks identical to page 102 in the manual
(8mil/25%/20mil) and I changed the default class to read 6mil/6mil/15mil, so
I think at a drill of 15mil the ring is 16mil and not 0mil.
I have see freeDFM get confused when you have a polygon over a via/pad.
freeDFM is complaining that all text associated with all (yes, all)
packages is too small. I've no idea how to fix that without editing the
respective libraries, since smashing isn't the answer.
-Ron
There are ULP's which fix it but that is one reason to have "your lib"
in which you copy all of the parts you need and fix them to your
requirements. After smashing you can group all of the text and change
the ratio. You may find that some of the silkscreen lines are too thin also.
Paul R.
"Paul Romanyszyn" <pgr@arcelectronicsinc.com> wrote in message
news:focl6b$5bf$1@cheetah.cadsoft.de...
I have see freeDFM get confused when you have a polygon over a via/pad.
Thanks for the reply, Paul! That's regarding freeDFM saying all my vias of
any size have an annular ring (restring) size of zero. I've not drawn any
polygons at all.
When I look at the freeDFM pictures it looks like all I have is via pads
with no drill holes, it all looks filled in. But in the board editor all
looks as it should. I did send an Excelon file to them. For one of the
pictured problem vias, the editor Info command gives me a report saying its
diameter is "0.031/0.031 (auto)" in inches, and I don't understand why it's
giving 2 parameters in those quotes but I do see that one divided by the
other does = zero and I wonder if that's the problem? For that via, the
drill is set at .015".
I've made the .brd file (only that file) available for anyone to see at:
http://www.RGMEusa.com/Misc/USBto64RW.zip
It doesn't include the silkscreen fixes, which I did on a different computer
last night. I only have the restring problem remaining. I don't think I can
fix it without doing a rip, so I'm not ripping until I understand the cause
of the vias problem with freeDFM.
-Ron
"Paul Romanyszyn" <pgr@arcelectronicsinc.com> wrote in message
news:focl6b$5bf$1@cheetah.cadsoft.de...
I have see freeDFM get confused when you have a polygon over a via/pad.
Thanks for the reply, Paul! That's regarding freeDFM saying all my vias of
any size have an annular ring (restring) size of zero. I've not drawn any
polygons at all.
When I look at the freeDFM pictures it looks like all I have is via pads
with no drill holes, it all looks filled in. But in the board editor all
looks as it should. I did send an Excelon file to them. For one of the
pictured problem vias, the editor Info command gives me a report saying its
diameter is "0.031/0.031 (auto)" in inches, and I don't understand why it's
giving 2 parameters in those quotes but I do see that one divided by the
other does = zero and I wonder if that's the problem? For that via, the
drill is set at .015".
I've made the .brd file (only that file) available for anyone to see at:
http://www.RGMEusa.com/Misc/USBto64RW.zip
It doesn't include the silkscreen fixes, which I did on a different computer
last night. I only have the restring problem remaining. I don't think I can
fix it without doing a rip, so I'm not ripping until I understand the cause
of the vias problem with freeDFM.
-Ron