EAGLE User Support (English) freeDFM & via issue
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
  • Replies 19 replies
  • Subscribers 177 subscribers
  • Views 1588 views
  • Users 0 members are here
Related

freeDFM & via issue

autodeskguest
autodeskguest over 17 years ago

I have a board I've submitted to freeDFM. Their error report for that board

is at:

.   https://www.freedfm.com/freedfm/0011385401921358/results/summary2.htm

The .brd file (only that file) I've made available at:

.   http://www.RGMEusa.com/Misc/USBto64RW.zip

 

I've already addressed all the issues not related to vias in another board

version, my only remaining problem is the one concerning freeDFM's complaint

about every one of the board vias.

 

If you look at the freeDFM error report it appears to my eye that all the

vias have no drill and they appear to all be filled in as if they were pads

instead of vias going through all 4 layers. I've also made available a

screen shot combination picture of the board concerning just one of the via

issues (the X=0.7641", Y=2.2966" example):

.   http://www.RGMEusa.com/Misc/SampleVia.jpg

 

It all seems ok to me so I haven't a clue as to why freeDFM is complaining.

In the combo screen shot I see it reports a drill for the example via as

0.015" and a diameter of "0.031/0.031 (auto)". I don't understand the

diameter syntax being used, meaning it looks to me like it is reporting 2

parameters separated by a "/" character. What is the definition of the 2

parameters which in the screen shot are identical to each other? If one

parameter is mathematically divided by the other the result is a zero value;

is THAT the reason freeDFM is complaining?

 

I need help understanding the nature of the problem and how to fix it. I did

generate the Execellon file while the board was displayed in the editor,

that's what was sent to freeDFM. TIA!

-Ron

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    Ron wrote:

    "Guy" <guy.dau_no_spam@free.fr> wrote in message

    news:foiedu$vrq$1@cheetah.cadsoft.de...

    "Ron" <Use@Forum.pls> a écrit dans le message de news:

    foicn5$rug$1@cheetah.cadsoft.de...

    "Guy" <guy.dau_no_spam@free.fr> wrote in message

    news:fohqh1$sgn$1@cheetah.cadsoft.de...

    Hi,

     

    When I'm testing it I have just one DRC error with design rule

    www.my4pcb.com you have select !!!

     

    Guy

     

    PS: I'm affray, you don't use any condensators on this card !!!

    I think you must minimum add decouplers condensators to be sure work ok

    !!!

    Yes, that version had too tight of clearance for those 2 pins - I

    corrected that already. Annoyed me, as when I auto routed that one trace

    the DRC rules were not followed and I had to move the trace manually one

    grid away from IC1. Luckily, there is a DRC check button!<smile>

     

    Guy, this design (and the hand wired proto) definitely does not need VCC

    bypass capacitors. It's a state machine, no clocking, and the USB module

    (it's not a chip) includes its own decoupling to the USB buss; what that

    module connects to is not powered by the USB buss and it is rather slow

    and usually just sitting in one state. I do, however, need to (or should)

    increase distance between the Power class traces. I gotta rip again

    anyhow when I find out why freeDRM doesn't like the vias, I'll change the

    class then.

    -Ron

    No !!

     

    It's not because it's a state machine and no clocking then decoupling is

    not necessary !!!

     

    With all these circuits and not decoupling, alimentation can start in

    resonance !!!

     

    With many TTL and CMOS you don't know alimentation reaction !!

     

    I think you must define any bypass/de-coupling and after perhaps not

    necessary to put all but you don't know !!!!!

     

    After many years of electronic developpement.......

     

    Sorry for my english,

     

    Guy

     

    This is getting way off topic but I do respect and appreciate your usage of

    English, please do not apologize. Although you could use a few less "!!!!!"

    characters!!!!! <vbg> You are understandable and if the situation were

    reversed I'd be, knowing only English, unable to return the courtesy.  But

    most of all I respect your knowledge.

     

    I would again try to qualify my agreement with what you say, which I believe

    to be a reference to a phenomenon known as parasitic resonance and which is

    a common annoyance in RF circuits. RF infers oscillation, and oscillating

    circuits have maximum power response at a resonant frequency.  My point is

    that there must be oscillation before there can be resonance, parasitic or

    not. This occurs in digital circuits primarily because of repeating patterns

    of current flow at high bit level changing rates (what I mean by "clocked",

    be it data pattern repetition or any other time base). The capacitive

    "decoupling" or "bypassing" is actually the detuning of the resonant

    circuit, dampening the amplitude of unintended oscillations to negligible

    level.  This is usually a very important consideration.

     

    But, if my design works (and the prototype does) and it experiences

    oscillations then it is malfunctioning because the amplitude of the

    oscillation would have to be of sufficient energy as to overpower the power

    supply as relates to the guaranteed high or low level specified for a gate

    input. If the power supply is working and distributed properly then that

    would have to be a rather huge amount of energy.  Without oscillation there

    can be no resonance.  If there can be no resonance then decoupling is not

    required.

     

    In this board all I/O is inherently latched. Even when changing at USB 2.0

    speed, the amount of time between cycles of a particular bit pattern that

    just happens to be resonant is what keeps enough energy from entering the

    tank to build sufficiently to overcome the power supply to a level where a

    gate would see a logic change. There simply aren't enough such cycles within

    a sufficiently small enough time period to build enough energy in a tank to

    sustain oscillation. If Murphy gets into the act regardless, then the

    mentioned time period can be lengthened by slowing down USB usage - thus

    detuning the tank.

     

    This board is an exception to the general rule that decoupling should be

    used. Primarily because it is latched and not clocked by some means.

    Repetitive tank pumping is not likely because repetitiveness does not exist

    in a latched circuit like it does in a clocked circuit. It would not hurt to

    use decoupling, except for production cost. My only worry with the entire

    design is that I might be exceeding the fan out rating of the USB module. If

    so, the resultant instability is not due to resonance or oscillation. On

    this board decoupling would be of little use, malfunction must begin before

    resonant oscillation can occur.

    -Ron

     

     

    Ron,

    Even low speed logic circuitry can generate transient oscillations due

    to the fast rise time of common digital ICs. This fast rise time causes

    the power supply to "see" sharp changes in demand for power, giving

    quite large voltage transients due to circuit inductance. This can

    propagate to adjacent circuits. The bypass capacitor provides this

    transient power to prevent or at least greatly reduce the spike on the

    supply line. I think you are being too optimistic that all will be well,

    just because the prototype worked OK.

    If this is a production board, with many to be made, tolerances could

    well give you a reasonable proportion which cause problems. It is

    easier, and not very expensive to add bypass capacitors at the start.

    John G.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    Ron wrote:

    "Guy" <guy.dau_no_spam@free.fr> wrote in message

    news:foiedu$vrq$1@cheetah.cadsoft.de...

    "Ron" <Use@Forum.pls> a écrit dans le message de news:

    foicn5$rug$1@cheetah.cadsoft.de...

    "Guy" <guy.dau_no_spam@free.fr> wrote in message

    news:fohqh1$sgn$1@cheetah.cadsoft.de...

    Hi,

     

    When I'm testing it I have just one DRC error with design rule

    www.my4pcb.com you have select !!!

     

    Guy

     

    PS: I'm affray, you don't use any condensators on this card !!!

    I think you must minimum add decouplers condensators to be sure work ok

    !!!

    Yes, that version had too tight of clearance for those 2 pins - I

    corrected that already. Annoyed me, as when I auto routed that one trace

    the DRC rules were not followed and I had to move the trace manually one

    grid away from IC1. Luckily, there is a DRC check button!<smile>

     

    Guy, this design (and the hand wired proto) definitely does not need VCC

    bypass capacitors. It's a state machine, no clocking, and the USB module

    (it's not a chip) includes its own decoupling to the USB buss; what that

    module connects to is not powered by the USB buss and it is rather slow

    and usually just sitting in one state. I do, however, need to (or should)

    increase distance between the Power class traces. I gotta rip again

    anyhow when I find out why freeDRM doesn't like the vias, I'll change the

    class then.

    -Ron

    No !!

     

    It's not because it's a state machine and no clocking then decoupling is

    not necessary !!!

     

    With all these circuits and not decoupling, alimentation can start in

    resonance !!!

     

    With many TTL and CMOS you don't know alimentation reaction !!

     

    I think you must define any bypass/de-coupling and after perhaps not

    necessary to put all but you don't know !!!!!

     

    After many years of electronic developpement.......

     

    Sorry for my english,

     

    Guy

     

    This is getting way off topic but I do respect and appreciate your usage of

    English, please do not apologize. Although you could use a few less "!!!!!"

    characters!!!!! <vbg> You are understandable and if the situation were

    reversed I'd be, knowing only English, unable to return the courtesy.  But

    most of all I respect your knowledge.

     

    I would again try to qualify my agreement with what you say, which I believe

    to be a reference to a phenomenon known as parasitic resonance and which is

    a common annoyance in RF circuits. RF infers oscillation, and oscillating

    circuits have maximum power response at a resonant frequency.  My point is

    that there must be oscillation before there can be resonance, parasitic or

    not. This occurs in digital circuits primarily because of repeating patterns

    of current flow at high bit level changing rates (what I mean by "clocked",

    be it data pattern repetition or any other time base). The capacitive

    "decoupling" or "bypassing" is actually the detuning of the resonant

    circuit, dampening the amplitude of unintended oscillations to negligible

    level.  This is usually a very important consideration.

     

    But, if my design works (and the prototype does) and it experiences

    oscillations then it is malfunctioning because the amplitude of the

    oscillation would have to be of sufficient energy as to overpower the power

    supply as relates to the guaranteed high or low level specified for a gate

    input. If the power supply is working and distributed properly then that

    would have to be a rather huge amount of energy.  Without oscillation there

    can be no resonance.  If there can be no resonance then decoupling is not

    required.

     

    In this board all I/O is inherently latched. Even when changing at USB 2.0

    speed, the amount of time between cycles of a particular bit pattern that

    just happens to be resonant is what keeps enough energy from entering the

    tank to build sufficiently to overcome the power supply to a level where a

    gate would see a logic change. There simply aren't enough such cycles within

    a sufficiently small enough time period to build enough energy in a tank to

    sustain oscillation. If Murphy gets into the act regardless, then the

    mentioned time period can be lengthened by slowing down USB usage - thus

    detuning the tank.

     

    This board is an exception to the general rule that decoupling should be

    used. Primarily because it is latched and not clocked by some means.

    Repetitive tank pumping is not likely because repetitiveness does not exist

    in a latched circuit like it does in a clocked circuit. It would not hurt to

    use decoupling, except for production cost. My only worry with the entire

    design is that I might be exceeding the fan out rating of the USB module. If

    so, the resultant instability is not due to resonance or oscillation. On

    this board decoupling would be of little use, malfunction must begin before

    resonant oscillation can occur.

    -Ron

     

     

    Ron,

    Even low speed logic circuitry can generate transient oscillations due

    to the fast rise time of common digital ICs. This fast rise time causes

    the power supply to "see" sharp changes in demand for power, giving

    quite large voltage transients due to circuit inductance. This can

    propagate to adjacent circuits. The bypass capacitor provides this

    transient power to prevent or at least greatly reduce the spike on the

    supply line. I think you are being too optimistic that all will be well,

    just because the prototype worked OK.

    If this is a production board, with many to be made, tolerances could

    well give you a reasonable proportion which cause problems. It is

    easier, and not very expensive to add bypass capacitors at the start.

    John G.