EAGLE User Support (English) Custom Library not in ADD list
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
  • Replies 1 reply
  • Subscribers 177 subscribers
  • Views 174 views
  • Users 0 members are here
Related

Custom Library not in ADD list

autodeskguest
autodeskguest over 17 years ago

First attempt at creating custom libraries.  I created a couple of test

libraries, all of which are using symbols copied from other libraries.  None

of the custom libraries are listed when I use the ADD command.

 

I have checked the following:

1. The custom libraries are in the same folder as all the other standard

libraries.

2. In EAGLE Control Panel, the radio button is green, indicating that the

custom library should be available to the ADD command.

3. However, I have found that in Control Panel, all other libraries will

have a sub-list of all the parts contained in the library.  My custom

libraries do not have any sub-list.

4.  Even though there are definitely symbols in the custom libraries that I

can edit, they do not appear to be recognized by EAGLE.

 

Any suggestions?  Worked on this for 4 hours already............THANKS!

 

 

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    TM wrote:

    First attempt at creating custom libraries.  I created a couple of test

    libraries, all of which are using symbols copied from other libraries.  None

    of the custom libraries are listed when I use the ADD command.

     

    I have checked the following:

    1. The custom libraries are in the same folder as all the other standard

    libraries.

    2. In EAGLE Control Panel, the radio button is green, indicating that the

    custom library should be available to the ADD command.

    3. However, I have found that in Control Panel, all other libraries will

    have a sub-list of all the parts contained in the library.  My custom

    libraries do not have any sub-list.

    4.  Even though there are definitely symbols in the custom libraries that I

    can edit, they do not appear to be recognized by EAGLE.

     

    Any suggestions?  Worked on this for 4 hours already............THANKS!

     

     

    A lib device requires both a symbol and footprint that are connected so

    is seems that your parts you have made(copied) are incomplete.

    Paul R.