First attempt at creating custom libraries. I created a couple of test
libraries, all of which are using symbols copied from other libraries. None
of the custom libraries are listed when I use the ADD command.
I have checked the following:
1. The custom libraries are in the same folder as all the other standard
libraries.
2. In EAGLE Control Panel, the radio button is green, indicating that the
custom library should be available to the ADD command.
3. However, I have found that in Control Panel, all other libraries will
have a sub-list of all the parts contained in the library. My custom
libraries do not have any sub-list.
4. Even though there are definitely symbols in the custom libraries that I
can edit, they do not appear to be recognized by EAGLE.
Any suggestions? Worked on this for 4 hours already............THANKS!