EAGLE User Support (English) Vista- files missing when searched for.
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
  • Replies 6 replies
  • Subscribers 178 subscribers
  • Views 526 views
  • Users 0 members are here
Related

Vista- files missing when searched for.

autodeskguest
autodeskguest over 17 years ago

Hello,

 

I just installed EAGLE on a Windows Vista Home Premium laptop.

 

I can create projects and schematics, boards, and gerber plots. However,

when I try to find them in explorer, they are gone. I open eagle and they

are there.

Also, any library files I create are there for editing. I then go to

Libraries - Use to add them. The operation appears to complete, but when I

try to use them, to add the parts to the schematic, they are not .in the

list. I can find the libraries in EAGLE, but they will not load as active.

-


I did find an answer to the help files not working. It works on my machine:

"Thank you for contacting Microsoft Customer Service.

I understand that you would like to know which WinHlp32.exe file you should

download.

I would like to inform you that x86 or x64 are platform for Windows Vista.

To find out the platform of the Windows Vista, please perform the following

steps:

- Click on "Start"

- Type in "System" in the Start Search box

- Click on System Information in the Programs list

- The "System type" option has the platform you are using

 

Jeffrey, for more information about finding the platform please visit the

article "How to determine whether your computer is running a 32-bit version

or a 64-bit version of the Windows operating system":

http://support.microsoft.com/kb/827218

 

After you determine the platform you are using, you may download the

appropriate WinHlp32.exe file from the web link below:

http://www.microsoft.com/downloads/details.aspx?FamilyId=6EBCFAD9-D3F5-4365-8070-334CD175D4BB&displaylang=en

"

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    Jack wrote:

    Jeffrey Moore wrote:

     

    "Jack" <jb46nospam@woh.rr.com> wrote in message

    news:fpka49$fu1$1@cheetah.cadsoft.de...

    Jeffrey Moore wrote:

    Hello,

     

    I just installed EAGLE on a Windows Vista Home Premium laptop.

     

    I can create projects and schematics, boards, and gerber plots.

    However, when I try to find them in explorer, they are gone. I open

    eagle and they are there.

    Also, any library files I create are there for editing. I then go to

    Libraries - Use to add them. The operation appears to complete, but

    when I try to use them, to add the parts to the schematic, they are

    not .in the list. I can find the libraries in EAGLE, but they will

    not load as active.

    ---------------------------------------------------------------------------------------------------

     

     

    I did find an answer to the help files not working. It works on my

    machine:

    "Thank you for contacting Microsoft Customer Service.

    I understand that you would like to know which WinHlp32.exe file you

    should download.

    I would like to inform you that x86 or x64 are platform for Windows

    Vista. To find out the platform of the Windows Vista, please perform

    the following steps:

    - Click on "Start"

    - Type in "System" in the Start Search box

    - Click on System Information in the Programs list

    - The "System type" option has the platform you are using

     

    Jeffrey, for more information about finding the platform please

    visit the article "How to determine whether your computer is running

    a 32-bit version or a 64-bit version of the Windows operating system":

    http://support.microsoft.com/kb/827218

     

    After you determine the platform you are using, you may download the

    appropriate WinHlp32.exe file from the web link below:

    http://www.microsoft.com/downloads/details.aspx?FamilyId=6EBCFAD9-D3F5-4365-8070-334CD175D4BB&displaylang=en

    "

     

     

     

    Vista is very protective of the Program Files directory. You're not

    supposed to store data there, such as your Projects directory.

     

    Your projects are most likely under 'Users\your_name\'. Use the

    Search to look for them, but be sure to choose the Advanced search,

    and Search the entire drive. Otherwise they will be missed. You may

    have to add the paths to your Options->Directories window just off

    the opening screen.

     

    Jack Butler

     

    You got it!  I will try changing the paths to be specific instead of

    "$EAGLEDIR\

    Tried:   c:\program files\eagle-rev\ for all directory settings. Still

    saves any

    and all new files in the 'Users\your_name\VirtualStore\Program Files\

    eagle-rev directory.

    Will try various configurations and get back to you.

     

    Jeffrey Moore

     

     

    Jeffrey...

     

    I wasn't at my Vista machine when I wrote the last message - this time I

    am.

     

    On my installation, the CAM, DOC, DRU, LBR, ULP, SCR directories are in

    the Program Files directory (not a good idea, but DOC is probably OK).

    Eaglerc.usr.beta is in C:\Users\your_name\AppData\Roaming\CadSoft\Eagle.

    The project files are in C:\Users\your_name\Documents\Eagle\Project.

    This last location requires that you add '$HOME\EAGLE' to your

    Options->Directories pop-up in Eagle (in the Project window).

     

    The problem with having libraries, scripts etc. in the Program Files

    directory is that Vista will refuse to download new libs or ulps etc.

    from the CadSoft website (or anywhere else for that matter). On-line or

    network access to Program Files is forbidden. The only way to get them

    downloaded is to make the download to another directory (I use

    'doctemp') and then copy or move them to the Program Files directory.

    Just a little added fuss.

     

    I'm going to try to move all of the auxiliary directories to the same

    location under Users with the Projects. Should work (I hope).

     

    HTH,

    Jack Butler

     

    OOPS!!! I just realized that I gave locations for the Beta version of

    Eagle. I don't have 4.16r2 installed on the Vista machine. (I'm

    currently moving everything from an 8 yr old laptop to a new one.)

     

    I think the file locations above should still be basically correct as

    the Beta version hasn't really changed the file access behavior from

    4.16. The big changes are in Vista's file structure.

     

    Ignore the location for eaglere.usr.beta. You won't have that file.

     

    Jack Butler

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    Jack wrote:

    Jeffrey Moore wrote:

     

    "Jack" <jb46nospam@woh.rr.com> wrote in message

    news:fpka49$fu1$1@cheetah.cadsoft.de...

    Jeffrey Moore wrote:

    Hello,

     

    I just installed EAGLE on a Windows Vista Home Premium laptop.

     

    I can create projects and schematics, boards, and gerber plots.

    However, when I try to find them in explorer, they are gone. I open

    eagle and they are there.

    Also, any library files I create are there for editing. I then go to

    Libraries - Use to add them. The operation appears to complete, but

    when I try to use them, to add the parts to the schematic, they are

    not .in the list. I can find the libraries in EAGLE, but they will

    not load as active.

    ---------------------------------------------------------------------------------------------------

     

     

    I did find an answer to the help files not working. It works on my

    machine:

    "Thank you for contacting Microsoft Customer Service.

    I understand that you would like to know which WinHlp32.exe file you

    should download.

    I would like to inform you that x86 or x64 are platform for Windows

    Vista. To find out the platform of the Windows Vista, please perform

    the following steps:

    - Click on "Start"

    - Type in "System" in the Start Search box

    - Click on System Information in the Programs list

    - The "System type" option has the platform you are using

     

    Jeffrey, for more information about finding the platform please

    visit the article "How to determine whether your computer is running

    a 32-bit version or a 64-bit version of the Windows operating system":

    http://support.microsoft.com/kb/827218

     

    After you determine the platform you are using, you may download the

    appropriate WinHlp32.exe file from the web link below:

    http://www.microsoft.com/downloads/details.aspx?FamilyId=6EBCFAD9-D3F5-4365-8070-334CD175D4BB&displaylang=en

    "

     

     

     

    Vista is very protective of the Program Files directory. You're not

    supposed to store data there, such as your Projects directory.

     

    Your projects are most likely under 'Users\your_name\'. Use the

    Search to look for them, but be sure to choose the Advanced search,

    and Search the entire drive. Otherwise they will be missed. You may

    have to add the paths to your Options->Directories window just off

    the opening screen.

     

    Jack Butler

     

    You got it!  I will try changing the paths to be specific instead of

    "$EAGLEDIR\

    Tried:   c:\program files\eagle-rev\ for all directory settings. Still

    saves any

    and all new files in the 'Users\your_name\VirtualStore\Program Files\

    eagle-rev directory.

    Will try various configurations and get back to you.

     

    Jeffrey Moore

     

     

    Jeffrey...

     

    I wasn't at my Vista machine when I wrote the last message - this time I

    am.

     

    On my installation, the CAM, DOC, DRU, LBR, ULP, SCR directories are in

    the Program Files directory (not a good idea, but DOC is probably OK).

    Eaglerc.usr.beta is in C:\Users\your_name\AppData\Roaming\CadSoft\Eagle.

    The project files are in C:\Users\your_name\Documents\Eagle\Project.

    This last location requires that you add '$HOME\EAGLE' to your

    Options->Directories pop-up in Eagle (in the Project window).

     

    The problem with having libraries, scripts etc. in the Program Files

    directory is that Vista will refuse to download new libs or ulps etc.

    from the CadSoft website (or anywhere else for that matter). On-line or

    network access to Program Files is forbidden. The only way to get them

    downloaded is to make the download to another directory (I use

    'doctemp') and then copy or move them to the Program Files directory.

    Just a little added fuss.

     

    I'm going to try to move all of the auxiliary directories to the same

    location under Users with the Projects. Should work (I hope).

     

    HTH,

    Jack Butler

     

    OOPS!!! I just realized that I gave locations for the Beta version of

    Eagle. I don't have 4.16r2 installed on the Vista machine. (I'm

    currently moving everything from an 8 yr old laptop to a new one.)

     

    I think the file locations above should still be basically correct as

    the Beta version hasn't really changed the file access behavior from

    4.16. The big changes are in Vista's file structure.

     

    Ignore the location for eaglere.usr.beta. You won't have that file.

     

    Jack Butler