EAGLE User Support (English) Linux appearance and behavior.
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
  • Replies 7 replies
  • Subscribers 179 subscribers
  • Views 522 views
  • Users 0 members are here
Related

Linux appearance and behavior.

autodeskguest
autodeskguest over 17 years ago

 

Hi,

 

I'm running Eagle under Debian AMD 64.

There are few problems:

 

1) the control panel tree and the menu bar are unusable. As you see in

the image attached, they appears with items duplicated. I experience

this only with Eagle.

 

2) When in then schematic window, the press of the schematic/layout

switch doesn't bring up the other window. I need to click it in the task

bar.

 

3) The appearance of Eagle windows are quite different than all other

application. See for example the Open Office example on the right.

Should it be possible to tell Eagle to follow the current desktop theme?

(yeah, this one is really not a big deal!)

 

Thanks

Marco / iw2nzm

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    Richard Hammerl wrote:

     

    Use a simple text editor to write the lines above and save it at any

    location with any name. Now you have to make the file executable,

    for example with

      chmod  +x  filename

     

    Now you can execute it in the command line ( ./filename ) or you can

    make a Desktop icon for it.

     

     

    Ok, I followed your instructions and I was able to launch the script.

    But Eagle appears exactly as before.

     

    Not a big problem, anyway.

     

    Marco / iw2nzm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    Richard Hammerl wrote:

     

    Use a simple text editor to write the lines above and save it at any

    location with any name. Now you have to make the file executable,

    for example with

      chmod  +x  filename

     

    Now you can execute it in the command line ( ./filename ) or you can

    make a Desktop icon for it.

     

     

    Ok, I followed your instructions and I was able to launch the script.

    But Eagle appears exactly as before.

     

    Not a big problem, anyway.

     

    Marco / iw2nzm