EAGLE User Support (English) Linux appearance and behavior.
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
  • Replies 7 replies
  • Subscribers 179 subscribers
  • Views 522 views
  • Users 0 members are here
Related

Linux appearance and behavior.

autodeskguest
autodeskguest over 17 years ago

 

Hi,

 

I'm running Eagle under Debian AMD 64.

There are few problems:

 

1) the control panel tree and the menu bar are unusable. As you see in

the image attached, they appears with items duplicated. I experience

this only with Eagle.

 

2) When in then schematic window, the press of the schematic/layout

switch doesn't bring up the other window. I need to click it in the task

bar.

 

3) The appearance of Eagle windows are quite different than all other

application. See for example the Open Office example on the right.

Should it be possible to tell Eagle to follow the current desktop theme?

(yeah, this one is really not a big deal!)

 

Thanks

Marco / iw2nzm

 

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Marco Trapanese wrote:

     

    As you see in the image attached

     

    Forgot to attach.

     

    M

     

     

    Attachments:
    image
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 17 years ago

    Marco Trapanese schrieb:

     

    Hi,

     

    I'm running Eagle under Debian AMD 64.

    There are few problems:

     

    1) the control panel tree and the menu bar are unusable. As you see in

    the image attached, they appears with items duplicated. I experience

    this only with Eagle.

     

    2) When in then schematic window, the press of the schematic/layout

    switch doesn't bring up the other window. I need to click it in the task

    bar.

     

    3) The appearance of Eagle windows are quite different than all other

    application. See for example the Open Office example on the right.

    Should it be possible to tell Eagle to follow the current desktop theme?

    (yeah, this one is really not a big deal!)

     

    Thanks

    Marco / iw2nzm

     

     

     

    Marco,there is no attachment, but could it have something to do

    with the composite extension?

     

    Please take look at our FAQ:

    http://www.cadsoft.de/faq.htm.en#07041701

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dukepro
    dukepro over 17 years ago

    Richard Hammerl wrote:

    Marco Trapanese schrieb:

    Hi,

     

    I'm running Eagle under Debian AMD 64.

    There are few problems:

     

    ...

    3) The appearance of Eagle windows are quite different than all other

    application. See for example the Open Office example on the right.

    Should it be possible to tell Eagle to follow the current desktop theme?

    (yeah, this one is really not a big deal!)

     

    Thanks

    Marco / iw2nzm

     

     

    Marco,there is no attachment, but could it have something to do

    with the composite extension?

     

    Please take look at our FAQ:

    http://www.cadsoft.de/faq.htm.en#07041701

     

    Marco,

     

    Can't help you with the behavior, but I can with the appearance.  I had

    the same problem a while back and was able to fix it with the following

    script:

     

         #!/bin/bash

         rm -r ~/.qt

         exec /opt/eagle/bin/eagle $*

     

    I placed this in ~/bin which is the first element in my PATH.

     

    Eagle does something with qT - not sure what or why, but this solves it.

     

    Enjoy,

         - Chuck

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Richard Hammerl wrote:

     

    Marco,there is no attachment

     

    I'm sorry. I forgot to attach to the first post. As you can see I added

    it later.

     

     

    but could it have something to do

    with the composite extension?

     

    Please take look at our FAQ:

    http://www.cadsoft.de/faq.htm.en#07041701

     

    I should check it before. Now this problem is fixed.

     

    Thanks,

    Marco / iw2nzm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Chuck Huber wrote:

     

    Marco,

     

    Can't help you with the behavior, but I can with the appearance.  I had

    the same problem a while back and was able to fix it with the following

    script:

     

        #!/bin/bash

        rm -r ~/.qt

        exec /opt/eagle/bin/eagle $*

     

    I placed this in ~/bin which is the first element in my PATH.

     

    Eagle does something with qT - not sure what or why, but this solves it.

     

     

    Chuck,

     

    thank you for your answer. I have no experience with linux systems, so I

    hope you don't blame me if I ask you how to create a script.

     

    I know it's a plain text file. I can save it in ~/bin with any name? It

    will be executed automatically?

     

    Thanks again

    Marco / iw2nzm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 17 years ago

    Marco Trapanese schrieb:

    Chuck Huber wrote:

     

    Marco,

     

    Can't help you with the behavior, but I can with the appearance.  I

    had the same problem a while back and was able to fix it with the

    following script:

     

        #!/bin/bash

        rm -r ~/.qt

        exec /opt/eagle/bin/eagle $*

     

    I placed this in ~/bin which is the first element in my PATH.

     

    Eagle does something with qT - not sure what or why, but this solves it.

     

    Chuck,

     

    thank you for your answer. I have no experience with linux systems, so I

    hope you don't blame me if I ask you how to create a script.

     

    I know it's a plain text file. I can save it in ~/bin with any name? It

    will be executed automatically?

     

    Thanks again

    Marco / iw2nzm

     

    Use a simple text editor to write the lines above and save it at any

    location with any name. Now you have to make the file executable,

    for example with

      chmod  +x  filename

     

    Now you can execute it in the command line ( ./filename ) or you can

    make a Desktop icon for it.

     

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Richard Hammerl wrote:

     

    Use a simple text editor to write the lines above and save it at any

    location with any name. Now you have to make the file executable,

    for example with

      chmod  +x  filename

     

    Now you can execute it in the command line ( ./filename ) or you can

    make a Desktop icon for it.

     

     

    Ok, I followed your instructions and I was able to launch the script.

    But Eagle appears exactly as before.

     

    Not a big problem, anyway.

     

    Marco / iw2nzm