EAGLE User Support (English) Placing vias
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
  • Replies 3 replies
  • Subscribers 178 subscribers
  • Views 577 views
  • Users 0 members are here
Related

Placing vias

autodeskguest
autodeskguest over 17 years ago

Hi,

 

I'm routing a double-side board with off-grid parts. I'm using the

finest grid beacuse the layout is very simple with straight lines.

 

When two traces overlap I place a via to connect each other. EAGLE

connects only one trace to the via, the trace on the other layer won't

be connected.

 

In fact, the overlap will lead a connection when the PCB will be made,

but for EAGLE it won't.

 

How to force a connection between two overlapping traces?

 

Thank

Marco / iw2nzm

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    David Pollum wrote:

    Marco Trapanese wrote:

    Hi,

     

    I'm routing a double-side board with off-grid parts. I'm using the

    finest grid beacuse the layout is very simple with straight lines

    If you get your parts on-grid, it makes routing easier and the > board looks nicer, too.  Normally, a 50 mil (thou) grid is used for > component placement, and smaller grids are used for routing traces.  If > you use metric, then I suppose the grid would be 0.5mm (?). >> >> When two traces overlap I place a via to connect each other. EAGLE >> connects only one trace to the via, the trace on the other layer won't >> be connected. >> >> In fact, the overlap will lead a connection when the PCB will be made, >> but for EAGLE it won't. >> >> How to force a connection between two overlapping traces? >> >> Thank >> Marco / iw2nzm > > Maybe I don't understand what you are talking about, but a via can

    only be used to join tracks on different layers that have the same

    net name (i.e. clock)

     

    -Dave Pollum

     

    Are you by any chance laying out a board without a corresponding

    schematic file?

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    David Pollum wrote:

    Marco Trapanese wrote:

    Hi,

     

    I'm routing a double-side board with off-grid parts. I'm using the

    finest grid beacuse the layout is very simple with straight lines

    If you get your parts on-grid, it makes routing easier and the > board looks nicer, too.  Normally, a 50 mil (thou) grid is used for > component placement, and smaller grids are used for routing traces.  If > you use metric, then I suppose the grid would be 0.5mm (?). >> >> When two traces overlap I place a via to connect each other. EAGLE >> connects only one trace to the via, the trace on the other layer won't >> be connected. >> >> In fact, the overlap will lead a connection when the PCB will be made, >> but for EAGLE it won't. >> >> How to force a connection between two overlapping traces? >> >> Thank >> Marco / iw2nzm > > Maybe I don't understand what you are talking about, but a via can

    only be used to join tracks on different layers that have the same

    net name (i.e. clock)

     

    -Dave Pollum

     

    Are you by any chance laying out a board without a corresponding

    schematic file?