EAGLE User Support (English) Additional traces with wire
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
  • Replies 6 replies
  • Subscribers 178 subscribers
  • Views 392 views
  • Users 0 members are here
Related

Additional traces with wire

autodeskguest
autodeskguest over 17 years ago

When I create additional traces with the wire command and connect them to a

net, the nets are still indicated as separate.  Is this normal?

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    Jack wrote:

     

    Chris Isaacson wrote:

     

    When I create additional traces with the wire command and connect them

    to a net, the nets are still indicated as separate.  Is this normal?

     

     

    Also be sure to use the 'NET' command to connect things up, NOT the

    'WIRE' command.

    Jack

     

    The "WIRE" command only draws LINES, not TRACES.  A TRACE connects

    pins/pads of parts.  A TRACE is associated with a NET name.  If you

    insist, a WIRE can be converted into a TRACE by NAMING the WIRE to an

    existing NET name.  Confusing, isn't it ?

    HTH

    -Dave Pollum

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    Jack wrote:

     

    Chris Isaacson wrote:

     

    When I create additional traces with the wire command and connect them

    to a net, the nets are still indicated as separate.  Is this normal?

     

     

    Also be sure to use the 'NET' command to connect things up, NOT the

    'WIRE' command.

    Jack

     

    The "WIRE" command only draws LINES, not TRACES.  A TRACE connects

    pins/pads of parts.  A TRACE is associated with a NET name.  If you

    insist, a WIRE can be converted into a TRACE by NAMING the WIRE to an

    existing NET name.  Confusing, isn't it ?

    HTH

    -Dave Pollum