Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) what are DFM considerations for SMD Component placement on both side of PCB
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 16 replies
  • Answers 5 answers
  • Subscribers 190 subscribers
  • Views 4142 views
  • Users 0 members are here
  • placement
  • eagle
  • twoside
  • dfm
Related

what are DFM considerations for SMD Component placement on both side of PCB

ravi_butani
ravi_butani over 7 years ago

I am designing tiny flight controller for smartphone controlled plane and drone... rev-0 of the same is approx 5cm x 5cm and all components on top as per pic below..

image

now I am trying to reduce size and weight of flight controller board by using WiFi SoC chip rather than module and  placing components on both side of board ...

Please suggest considerations for placing components on both side of PCB board so it can be made by machine (Automatic placement and reflow machine)

 

Key Parts:

ESP32-PICO-D4 chip QFN

CP2102 USB-UART chip QFN

MPU6050 ACC-GYRO QFN

Misc-SMD LEDs, Resistors, Diodes, Caps, LDOs, BJTs, MOSFETs

 

 

Thanks,

 

Ravi

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 7 years ago

    Here is a guideline to follow :Component Layout Considerations – PCB DFM Part 4 | Seeed Studio Blog

    or maybe https://www.smta.org/chapters/files/Arizona-Sonora_Design_for_Manufacturing_-_Adan_Ortiz.pdf

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 7 years ago in reply to clem57

    5.9 COMPONENTS NOT RECOMMENDED FOR BOTTOM PLACEMENT

     

     

    Some types of components are sensitive to the higher temperatures of wave soldering and should not be used on the bottom of boards where the solder wave would contact the component. Other types of components may not be suited to wave solder because

    of their lead configurations and size. The following is a list of components to avoid placing on the bottom of a board to be wave soldered:

    Large body chip caps, package types 1812 and 1825 may crack when exposed to wave solder.

    Memory and static ram chips which may be damaged by high temperatures.

    The 1206 should be the smallest package size used on the solder side of the board. Smaller packages such as the 0805 are not well suited for epoxy application and wave solder.

    PLCCs as the lead configuration is not suited to wave solder.

    SOTs do not solder well due to leads being too close to component body.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 7 years ago in reply to clem57

    5.9 COMPONENTS NOT RECOMMENDED FOR BOTTOM PLACEMENT

     

     

    Some types of components are sensitive to the higher temperatures of wave soldering and should not be used on the bottom of boards where the solder wave would contact the component. Other types of components may not be suited to wave solder because

    of their lead configurations and size. The following is a list of components to avoid placing on the bottom of a board to be wave soldered:

    Large body chip caps, package types 1812 and 1825 may crack when exposed to wave solder.

    Memory and static ram chips which may be damaged by high temperatures.

    The 1206 should be the smallest package size used on the solder side of the board. Smaller packages such as the 0805 are not well suited for epoxy application and wave solder.

    PLCCs as the lead configuration is not suited to wave solder.

    SOTs do not solder well due to leads being too close to component body.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • michaelkellett
    0 michaelkellett over 7 years ago in reply to clem57

    Hey Clem, that's a bit out of date !

     

    I think Ravi will be into 0402 and a PLCC would be bigger than his drone image (well, not quite).

     

    It's much more common with fine pitch work to use solder paste and reflow on both sides of the board.

     

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 7 years ago in reply to clem57

    Am 18.09.2019 um 15:45 schrieb BB-Sphere (Clem):

    h4. 5.9 COMPONENTS NOT RECOMMENDED FOR BOTTOM PLACEMENT

     

     

    Some types of components are sensitive to the higher temperatures of wave soldering and should not be used on the bottom of boards where the solder wave would contact the component. Other types of components may not be suited to wave solder because

    of their lead configurations and size. The following is a list of components to avoid placing on the bottom of a board to be wave soldered:

    Large body chip caps, package types 1812 and 1825 may crack when exposed to wave solder.

    Memory and static ram chips which may be damaged by high temperatures.

    The 1206 should be the smallest package size used on the solder side of the board. Smaller packages such as the 0805 are not well suited for epoxy application and wave solder.

    PLCCs as the lead configuration is not suited to wave solder.

    SOTs do not solder well due to leads being too close to component body.

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/281746

     

     

      Maybe two single sided with minor edge connections between them can be

    done?

    as Morton suggested...

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag