EAGLE User Support (English) what are DFM considerations for SMD Component placement on both side of PCB
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
  • State Suggested Answer
  • Replies 16 replies
  • Answers 5 answers
  • Subscribers 182 subscribers
  • Views 3577 views
  • Users 0 members are here
  • placement
  • eagle
  • twoside
  • dfm
Related

what are DFM considerations for SMD Component placement on both side of PCB

ravi_butani
ravi_butani over 6 years ago

I am designing tiny flight controller for smartphone controlled plane and drone... rev-0 of the same is approx 5cm x 5cm and all components on top as per pic below..

image

now I am trying to reduce size and weight of flight controller board by using WiFi SoC chip rather than module and  placing components on both side of board ...

Please suggest considerations for placing components on both side of PCB board so it can be made by machine (Automatic placement and reflow machine)

 

Key Parts:

ESP32-PICO-D4 chip QFN

CP2102 USB-UART chip QFN

MPU6050 ACC-GYRO QFN

Misc-SMD LEDs, Resistors, Diodes, Caps, LDOs, BJTs, MOSFETs

 

 

Thanks,

 

Ravi

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 6 years ago in reply to clem57 +4 suggested
    Hey Clem, that's a bit out of date ! I think Ravi will be into 0402 and a PLCC would be bigger than his drone (well, not quite). It's much more common with fine pitch work to use solder paste and reflow…
  • geralds
    geralds over 6 years ago +2 suggested
    If I now take your picture as an approach (as I see it's a 2-sided board), I suggest you can place all the resistors and capacitors, transistors on the bottom side. The ICs, the module and the connectors…
  • michaelkellett
    michaelkellett over 6 years ago in reply to ravi_butani +2 suggested
    Placement on both sides will cost more - if you put only small parts on one side not too much more, if you put heavy parts on both sides then costs will rocket because they will need to be glued. The rule…
  • ravi_butani
    0 ravi_butani over 6 years ago

    Also does placement of components on both side compared to one side makes any difference in assembly cost?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • geralds
    0 geralds over 6 years ago

    If I now take your picture as an approach (as I see it's a 2-sided board), I suggest you can place all the resistors and capacitors, transistors on the bottom side.

    The ICs, the module and  the connectors can be placed on the top side.

    Then the board gets smaller and if you also pay attention to the mounting holes, I see no problems with the assembly of the board.

    You can mill out the board with fingers for the mounting holes, so that it can be directly mounted on the drone.

    Or you can assemble with fasteners, e.g. large screws, or mounting brackets to the board.

     

    Assembly cost I think will be marginal, plus-minus...

     

    Best Regards

    Gerald

    ---

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 6 years ago in reply to ravi_butani

    Placement on both sides will cost more - if you put only small parts on one side not too much more, if you put heavy parts on both sides then costs will rocket because they will need to be glued.

     

    The rule is  - talk to the assembly engineer before you commit yourself.

     

    How many will you make - if its just a few it doesn't matter.

     

    Be very careful about putting any parts under the RF chips/modules - there will be rules in the data sheet.

     

    Are you sure you can design an RF module better (smaller, lighter) than people who make millions of them - do you have the RF test gear etc.

    You might do better to stick with the module (get the lightest one you can) and minimise the

    size and weight of all the other stuff.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ravi_butani
    0 ravi_butani over 6 years ago in reply to michaelkellett

    I Appreciate quick and very helpful response...

    Regarding module, I will use ESP32-PICO-D4 chip which is having all RF parts (balun, crystal etc..) on chip. I just need to trace UFL connecter for external antenna or proven PCB layout for WiFi Antenna.. and datasheet is very clear about PCB layout guidelines so decided to giving it a try...

     

    Thanks Again,

     

    Ravi

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ravi_butani
    0 ravi_butani over 6 years ago in reply to geralds

    Confusion almost cleared.. and now ready to bashing on to the PCB Layout...Will share results..

    Thanks a lot....

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 6 years ago in reply to ravi_butani

    I'll be interested to hear how it works out !

     

    Good luck.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • geralds
    0 geralds over 6 years ago in reply to ravi_butani

    For example, if you place a resistor (or other warming components) underneath the RF module on the bottom, this resistor can heat the module up.

    That's what you have to see too. Or RF parameters could change because such components cause EMC problems.

     

    Sticking the components on the bottom is relatively, nominally correct.

    There are solders that can hold the component well. But, it works only on small components.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ravi_butani
    0 ravi_butani over 6 years ago in reply to geralds

    Sure... will take care of the same...

    In fact.... I need more care while preparing layout coz many of the parts may introduce interference i.e. motor driver mosfets carrying high frequency (33kHz) switching current in Amp (1Amp to 2Amp) on board...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • geralds
    0 geralds over 6 years ago in reply to ravi_butani

    Yes, yes, yes, image.... Well, it's a fine job. Good luck!

    One tipp image: reserve a landing area place for your big cup of coffee!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • geralds
    0 geralds over 6 years ago in reply to ravi_butani

    One I forgotten to mention, for making smaller the weight:

    For the mounting brackets, screws, or so, you can also select the materials e.g. plastics instead of metals.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>