EAGLE User Support (English) Analog and digital ground; how to connect?
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
  • Replies 5 replies
  • Subscribers 178 subscribers
  • Views 1740 views
  • Users 0 members are here
Related

Analog and digital ground; how to connect?

autodeskguest
autodeskguest over 17 years ago

Hi,

 

I have a circuit which uses an analog and digital ground.

 

These grounds must be connected at one point. How can i achieve this?

 

Note:

I created a dgnd and an agnd ; i connected these two symbols in the

schematic; it results in a net of agnd or dgnd; The electric rule check

results in an ERROR: .... overwritten with more than one signal .

 

 

Regards,

 

Johan

 

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Familie Maas ha scritto:

     

    I have a circuit which uses an analog and digital ground.

     

    These grounds must be connected at one point. How can i achieve this?

     

    Note:

    I created a dgnd and an agnd ; i connected these two symbols in the

    schematic; it results in a net of agnd or dgnd; The electric rule check

    results in an ERROR: .... overwritten with more than one signal .

     

     

    Try supply-dummy.lbr

     

    Marco / iw2nzm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Marco Trapanese wrote:

    Familie Maas ha scritto:

     

    I have a circuit which uses an analog and digital ground.

     

    These grounds must be connected at one point. How can i achieve this?

     

    Note:

    I created a dgnd and an agnd ; i connected these two symbols in the

    schematic; it results in a net of agnd or dgnd; The electric rule

    check results in an ERROR: .... overwritten with more than one signal .

     

    Try supply-dummy.lbr

     

    Marco / iw2nzm

     

    Can't see that on cadsoft's site

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Peter Harrison ha scritto:

     

    Can't see that on cadsoft's site

     

    I have it in the lbr folder by default.

     

    Marco / iw2nzm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Some remarks:

     

    AVAILABILITY

    In release 4.16r2 it is present. (in my older release 4.13r2 it was also not

    available)

     

    HOW WILL IT WORK?

    But i dont get the point how it works.

    After adding the component to the schematic the component is also present on

    the board (two pads).

    Between the two pads a component (for example a resistor of 0 ohm) must be

    soldered to make the connection between the two nets. Is that the idea?

     

     

    LAYERS NOT PRESENT

    The help says "Ground connector display layer 53 (54) to make copper (route)

    from gnd to gnda"

     

    The layers 53 and 54 are not available at all?

     

    Hope to get some clarrification?

     

    Regards,

     

    Johan

     

     

    "Marco Trapanese" <marcotrapaneseNOSPAM@gmail.com> schreef in bericht

    news:fs2bqo$tb0$1@cheetah.cadsoft.de...

    Peter Harrison ha scritto:

     

    Can't see that on cadsoft's site

     

    I have it in the lbr folder by default.

     

    Marco / iw2nzm

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Familie Maas wrote:

    Hi,

     

    I have a circuit which uses an analog and digital ground.

     

    These grounds must be connected at one point. How can i achieve this?

     

    Note:

    I created a dgnd and an agnd ; i connected these two symbols in the

    schematic; it results in a net of agnd or dgnd; The electric rule

    check results in an ERROR: .... overwritten with more than one signal

    .

     

    Regards,

     

    Johan

     

    I've handled this by creating a library part with two pins in the schematic

    symbol.  For the footprint, I place two pads on top of each other (either

    SMT or through-hole).

     

    You can use this part in your schematic, connecting AGND to one pin and DGND

    to the other pin.  In the layout, you will neatly get the pad with an air

    wire to both AGND and DGND, but no other air wires between AGND and DGND.

     

    Of course, DRC will complain loudly about the overlapping pads.  I always

    look through the list of errors, and ignore the ones relating to the

    overlapping pads.

     

    --

    Bert Menkveld