Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Problems installing version 4.16r2
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 186 subscribers
  • Views 679 views
  • Users 0 members are here
Related

Problems installing version 4.16r2

autodeskguest
autodeskguest over 18 years ago

Hi

 

I have recently reinstalled windows 2000 on a new computer, but ran into

a problem when installing Eagle v4.16r2.

After nearly finished installation I get the following message on file

INS0432.MP

 

"The file or directory is corrupt or unreadable. Please run chkdsk utility"

 

After accepting this message i get a new message being almost identical,

locking like this (difference in bold)

 

"The file or directory C: is corrupt or unreadable. Please run chkdsk

utility"

 

The program seems to run as it should but the message worries me since I

cant detect any errors on my computer using any disk utilities (and I

have a few).

System information:

OS: Windows 2000 SP4 version 5.00.2195 English

File system: NTFS

RAM: 1GB

Chipset: Intel 945

CPU: Pentium 4 (3GHz)

 

Only thing that comes to my mind is that I changed the default

allocation for Eagle to c:\Program files\cadsoft\eagle

 

I have earlier run same version on same HW using w2k (before re

installation).

Note: Reason for me to reinstall is  that I earlier, last week, tried to

install and try out the  BETA 5 version of Eagle but the computer

crashed during installation and I never got the system stable again.

(see news://news.cadsoft.de:119/frlbo5$jjr$1@cheetah.cadsoft.de)

 

I tried to download the installation file for version 4.16r2 again and

reinstall it but with the same result.

 

I am keeping the option "local HW failure" in my mind being concerned

for my HDD, but so far I cant understand that it is Eagle that every

time is the trigger  for these abnormalities.

 

I use quite many development sw tool chains on this computer and none of

theme seems to give me any troubles like these.

 

What is the INS0432.MP ? It seems that there is problems related to

extracting this file...

 

 

Thanks in advance.

 

Best regards

Vidar

 

  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    Richard_H over 18 years ago

    zainka schrieb:

     

     

     

    By the way, what could the temp directory have to do with this???

     

    breg

    Vidar (Z)

     

     

    The InstallShield uses the temp directory for storing and reading

    files while the installing process, as most other applications

    do. But not all setup routines delete their temporary files after

    finishing the installation process.

    Now it may happen that InstallShield wrongly recoginizes some

    left over files. This can cause problems for the installation

    process.....

    So it is wise to delete all temp files before.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 18 years ago

    zainka schrieb:

     

     

     

    By the way, what could the temp directory have to do with this???

     

    breg

    Vidar (Z)

     

     

    The InstallShield uses the temp directory for storing and reading

    files while the installing process, as most other applications

    do. But not all setup routines delete their temporary files after

    finishing the installation process.

    Now it may happen that InstallShield wrongly recoginizes some

    left over files. This can cause problems for the installation

    process.....

    So it is wise to delete all temp files before.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
No Data