Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) DRC clearance error
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Subscribers 188 subscribers
  • Views 1087 views
  • Users 0 members are here
Related

DRC clearance error

nav101
nav101 over 6 years ago

I am using a library for MCP73871 battery controller. I tried two different librarys but I get the same clearance error as shown in the picture. This is qfn package where the centre is the exposed pad and is grounded.

Changing DRC clearance does not get rid of the error. Is it a faulty library or am i doing something wrong ... MANY THANKSimage

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 6 years ago

    On 05/11/2019 17:41, Nav Khan wrote:

    I am using a library for MCP73871 battery controller. I tried two different librarys but I get the same clearance error as shown in the picture. This is qfn package where the centre is the exposed pad and is grounded.

    Changing DRC clearance does not get rid of the error. Is it a faulty library or am i doing something wrong ... MANY THANKS

     

    There are two separate issues here.

     

    First, the four thermal vias in the centre pad are misaligned such that

    one of them is practically touching pin 13. You need to re-centre them.

    They're also not being recognised as ground vias, by the look of it,

    although the airwires suggest they are correctly named. Which version of

    Eagle are you using? I think the rules changed at some point.

     

    Second, you've got pad-to-pad clearance settings in your DRC rules that

    don't allow for this footprint. I'm not familiar with the device in

    question so I can't say whether the centre pad really needs to be as

    large as it is, or whether you need a board house that can manage very

    small clearances.

     

    In practice, even if those clearances are OK for manufacture, you may

    well need to adjust (or remove and hand-craft) the automatic solder mask

    on all the pads of a device like that.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • nav101
    0 nav101 over 6 years ago in reply to autodeskguest

    Hi Thanks for the response.

    The vias are non issue as I just added them to check if that would help in the clearance. So the clearance issue is still there even without the vias. I am new to this and this is my first design, I was really under the impression that the librarys available online are accurate. The manufacturing view of the device shows the central pad so large that it is touching the other surrounding pads. I should get down to designing my library...Thanks again

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 6 years ago in reply to nav101

    On 05/11/2019 18:58, Nav Khan wrote:

    I am new to this and this is my first design, I was really under the impression that the librarys available online are accurate. The manufacturing view of the device shows the central pad so large that it is touching the other surrounding pads. I should get down to designing my library...Thanks again

     

    So, first lesson... never trust anybody else's library! This is a rule

    that those of us who use Eagle a lot (or, indeed, use any other PCB CAD

    software in a professional environment) find ourselves repeating on the

    user forum. You cannot trust what you find on the web, to the point that

    it's usually quicker just to create the part yourself than search,

    download, and verify.

     

    If you're experiencing differences between the library and the board,

    this is something of an FAQ. It's down to DRC rules. However, this is

    mostly an issue for through-hole components, where the "annular ring"

    setting plays havoc with newbies' expectations. In essence, the library

    defines the minimum sizes needed for the component, while the DRC rules

    define the capabilities of the board house for that project. If the

    board house can't achieve the ultra-thin copper ring that the library

    defines for a PTH pad, the board gets a fatter one. I wouldn't expect

    that to be your problem as it doesn't normally affect SMD pads.

     

    The manufacturing preview may not always be fully accurate. Autodesk

    generally say that, where there is a discrepancy, the board editor is

    the one to trust. Or you can generate Gerber files and open them in

    something like gerbv, which should be definitive.

     

    BTW, the Element14 forum, and the old CadSoft NNTP server it's linked

    to, are not the best place for Eagle advice any more. You'd get a better

    spread of response (including official support) from the Autodesk forum

    at https://forums.autodesk.com/t5/eagle-forum/bd-p/3500

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • nav101
    0 nav101 over 6 years ago in reply to autodeskguest

    Joern, the minimum is actually 2.6x2.6mm and I did exactly what you said and it got rid of the clearance error.

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • nav101
    0 nav101 over 6 years ago in reply to autodeskguest

    Joern, the minimum is actually 2.6x2.6mm and I did exactly what you said and it got rid of the clearance error.

    Thanks