EAGLE User Support (English) Mounting Plated Through Holes
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
  • Replies 1 reply
  • Subscribers 178 subscribers
  • Views 268 views
  • Users 0 members are here
Related

Mounting Plated Through Holes

autodeskguest
autodeskguest over 17 years ago

Hello!

 

See attached file that goes with the following message.

 

I used the VIA function to make four (4) mounting plated through hole

connected to ground. I renamed the VIA's to GND. The polygon (pour function)

also called GND.

 

My question is : "Is it the right appproach to do such thing?" ... In the

Library "Holes" the mounting holes are producing isolated mounting holes and

I want grounded holes.

 

Thank you for your help.

 

Regards,

 

RJ

 

 

 

 

Attachments:
imageMounting plated through holes .pdf
  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    RJ wrote:

    Hello!

     

    See attached file that goes with the following message.

     

    I used the VIA function to make four (4) mounting plated through hole

    connected to ground. I renamed the VIA's to GND. The polygon (pour

    function) also called GND.

     

    My question is : "Is it the right appproach to do such thing?" ... In

    the Library "Holes" the mounting holes are producing isolated

    mounting holes and I want grounded holes.

     

    Thank you for your help.

     

    Regards,

     

    RJ

     

    That approach seems fine to me, as long as you keep solder mask off your

    vias.

     

    What I do is to make a very simple library part, consisting of a single pad

    with the drill size and diameter I want for my mounting holes.  I add as

    many of these to my schematic as I need for the board.  The advantage of

    this is that the schematic shows the mounting holes and what net they

    connect to.  It also ensures there won't be any solder mask over the

    mounting hole pads, regardless of whether you want solder mask on your vias

    or not.

     

    --

    Bert Menkveld

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    RJ wrote:

    Hello!

     

    See attached file that goes with the following message.

     

    I used the VIA function to make four (4) mounting plated through hole

    connected to ground. I renamed the VIA's to GND. The polygon (pour

    function) also called GND.

     

    My question is : "Is it the right appproach to do such thing?" ... In

    the Library "Holes" the mounting holes are producing isolated

    mounting holes and I want grounded holes.

     

    Thank you for your help.

     

    Regards,

     

    RJ

     

    That approach seems fine to me, as long as you keep solder mask off your

    vias.

     

    What I do is to make a very simple library part, consisting of a single pad

    with the drill size and diameter I want for my mounting holes.  I add as

    many of these to my schematic as I need for the board.  The advantage of

    this is that the schematic shows the mounting holes and what net they

    connect to.  It also ensures there won't be any solder mask over the

    mounting hole pads, regardless of whether you want solder mask on your vias

    or not.

     

    --

    Bert Menkveld