EAGLE User Support (English) Library Inconsistent
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
  • Replies 4 replies
  • Subscribers 178 subscribers
  • Views 306 views
  • Users 0 members are here
Related

Library Inconsistent

autodeskguest
autodeskguest over 17 years ago

I am having a major headache over this right now.  Please bear with me

as I painstakingly TRY to tell you what the heck is going on here.

 

In a nutshell, I've updated my package layout to a particular part in

the library I am using, and when I hit "Update All" only a portion of my

components actually update.

 

When I check the info they are all listed as being from the same library.

 

When I search my computer there is only ONE copy of that library, I even

moved the .l## files to the recycle bin.

 

This problem is existing with the newer parts that I have placed.  There

was obviously some cross-over point in time for parts that seem to come

from a now non-existent library.

 

Since the creation of this library I have added some packages to my

devices, for instance, I added a 1206.a which has slight modifications

over my old, regular 1206 package information.  I added it to the device

and made the connections.  Once in either the schematic or the board I

can do a "change package" and see the three or more package options I

have for resistors... but ONLY for the newest ones.  For the older ones

only my original package option remains.  Furthermore when I look at

info on the older, non-updatable parts, instead of reading: "Package:

1206" they read "Package:1206@1" which is definitely no package I have

ever created.

 

My only guess is that EAGLE stores a copy of necessary library

information in the .sch and/or .brd files themselves.  I suspect this

b/c I've transported my files to computers that did not have my

libraries and everything showed up fine.  Somehow EAGLE must have

assumed that my library no longer existed when I moved my .sch file to

another system, even though I moved the library file with it.  After

doing that and moving back to the original system EAGLE must have

decided again to use some in-schematic-stored version of my libraries.

 

How in the heck can I get EAGLE to actually USE the library it's

supposed to have been using all along?

 

How did this happen?

 

WHY did this happen?

 

 

PLEASE HELP!

 

-jh

 

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 17 years ago

    before update all: use *, enter (command line)

    after that: all libs are in use

    r

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 17 years ago

    before update all: use *, enter (command line)

    after that: all libs are in use

    r