EAGLE User Support (English) Autorouter
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
  • Replies 1 reply
  • Subscribers 177 subscribers
  • Views 174 views
  • Users 0 members are here
Related

Autorouter

autodeskguest
autodeskguest over 17 years ago

Hi,

 

Does anyone know what is the "Best" Autorouter configuration? I only have

the Default2.ctl and the Myboardfilename.ctl versions to play with.

 

Typically my board complexity is as follows:-

 

70 x 60 mm size board

200 x SMD pads

25 x thru hole components

 

with settings :-

 

8 mil clearances

8 mil track width,

20 mil minimum drill

12 mil Restring Pads

8 mil Restring Vias

 

This gives me 110 x Vias  -using default2.ctl

 

I want to reduce the number of Vias to a bare minimum.

 

I have tried all types of moving components in different positions and

different sides of the board, etc. and 110 Vias is about the best I can get

without reducing the tolerances too much.

 

Can Anyone recommend any alternative Autorouter configurations that may be

better than my two?

 

With Thanks,

 

GunJet

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    FI schrieb:

    I need the supply pins thicker on the PCB. Is it possible to adhjust it

    in the autorouter. Ex: +15V,-15V minimum 20mil.

     

    just 2 words:  help class

     

     

    Thanks

    FI

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    FI schrieb:

    I need the supply pins thicker on the PCB. Is it possible to adhjust it

    in the autorouter. Ex: +15V,-15V minimum 20mil.

     

    just 2 words:  help class

     

     

    Thanks

    FI