EAGLE User Support (English) PortableApps
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
  • Replies 7 replies
  • Subscribers 177 subscribers
  • Views 785 views
  • Users 0 members are here
Related

PortableApps

autodeskguest
autodeskguest over 17 years ago

Hello,

 

it would be nice if EAGLE will be released also as a PortableApps

software (http://portableapps.com/). So we can open and change our

designs everywhere without carry out our notebook but just a USB pen. Of

course the license terms will be the same: only one person may use the

software.

 

Another stuff I think it could be very useful is an EAGLE viewer (free

software) so we can show and explore both schematics and boards to our

customers without exporting them as images or pdf files.

 

Please, leave a feedback here if you are either agree or disagree.

 

 

Marco / iw2nzm

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    Nicola ha scritto:

     

    Hi,

    I've just read your post: about the PortableApps it could be nice, even

    if I've never used USB pens like that.

     

    About the free viewer: isn't this allowed with the freeware version? I

    mean, even a bigger design, with more sheets / layers and so on, is

    possible to be seen (not edited) with the freeware version. Or am I

    missing something?

     

     

    Yes, with the freeware version you can open any design. But it would be

    nice a light viewer without any library, commands or other stuff. A

    single exe which doesn't need to be installed and that open any design

    in read-only mode.

     

    It's not useful to have the complete program when you won't use a lot of

    features!

     

    IMHO, of course image

     

    Marco / iw2nzm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    Nicola ha scritto:

     

    Hi,

    I've just read your post: about the PortableApps it could be nice, even

    if I've never used USB pens like that.

     

    About the free viewer: isn't this allowed with the freeware version? I

    mean, even a bigger design, with more sheets / layers and so on, is

    possible to be seen (not edited) with the freeware version. Or am I

    missing something?

     

     

    Yes, with the freeware version you can open any design. But it would be

    nice a light viewer without any library, commands or other stuff. A

    single exe which doesn't need to be installed and that open any design

    in read-only mode.

     

    It's not useful to have the complete program when you won't use a lot of

    features!

     

    IMHO, of course image

     

    Marco / iw2nzm