Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Can't find MY Library Folder
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 189 subscribers
  • Views 5776 views
  • Users 0 members are here
Related

Can't find MY Library Folder

celestine
celestine over 6 years ago

Hello   I  m totally new to Eagle but I have used Autodesk's TinkerCad   so I have use some CAD (however basic) before.

 

I am totally frustrated with even the most basics ops of Eagle.

I tried to draw a new schematic, so I selected <NEW> and <schematic>.

I went to ADD (a part) and I cannot find MY library.

The only library that opens is the Eagle one (managed).

How do I find MY library folder after hitting ADD?

I know it's there because I can see it in the control panel. Thanks

 

OK...so I found the part (Nixie Tube 1n-14)  and I want to use the "pin-out" pattern (Shown in the upper right corner)

But when I hit OK the other pattern is used, the one in Red (and I don't even know what that is).

So how can I get the tube pin out pattern onto my schematic? Thanks

 

image

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 6 years ago

    Am 14.07.2020 um 06:55 schrieb Patricia Hann:

    Hello   I  m totally new to Eagle but I have used Autodesk's TinkerCad   so I have use some CAD (however basic) before.

     

    I am totally frustrated with even the most basics ops of Eagle.

    I tried to draw a new schematic, so I selected <NEW> and <schematic>.

    I went to ADD (a part) and I cannot find MY library.

    The only library that opens is the Eagle one (managed).

    How do I find MY library folder after hitting ADD?

    I know it's there because I can see it in the control panel. Thanks

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/294064

     

     

    Hi Patricia,

    basically in a first statement you should mention your operating system

    and the eagle version so others know "what you are talking about" image

     

      In windows basically in control-panel/options you should place the

    paths to your libraries separated by semicolons.

    I'm using a non AD-Version of eagle, so I don't know if MY lib exist

    from beginning or it must be created by you, In any case check the

    control panel options.

     

    btw. hit F1 key for help

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • celestine
    0 celestine over 6 years ago in reply to autodeskguest

    Im using Windows 10

    Eagle 9.6.2

     

    As for the rest of what you said to do....really I have no idea what you telling me to do.

    Shouldn't I be able to click on "libraries" tab at the top of the schematic page and just open the folder I need?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • celestine
    0 celestine over 6 years ago in reply to autodeskguest

    Im using Windows 10

    Eagle 9.6.2

     

    As for the rest of what you said to do....really I have no idea what you telling me to do.

    Shouldn't I be able to click on "libraries" tab at the top of the schematic page and just open the folder I need?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • dukepro
    0 dukepro over 6 years ago in reply to autodeskguest

    Warren,

     

    Excellent point, and right you are!  I very rarely use "Update All". 

    Bringing it up escaped me at the time.

     

    Enjoy,

        - Chuck

     

     

     

    On 7/17/20 21:31, Warren Brayshaw wrote:

    On 17/07/2020 2:07 am, Chuck Huber wrote:

     

    For example: suppose Eagle's rcl.lbr contains a resistor, and your

    personal library does to.  When your design is updated from your

    personal library, only resistors that were sourced from your personal

    library will be affected.  The resistors in your design that were

    sourced from Eagle's rcl.lbr will not be affected.

     

    HI Chuck, this is not the full story if you don't specify the library

    and use "Update all"

     

    In this case a design will be updated from the first library Eagle

    finds with the correct library name with a matching device within it.

     

    So, when you set up Control Panel > Directories > Libraries, the order

    of the library paths is the order Eagle uses and as soon as it gets a

    Library/Device match it updates the design using that device because

    the library/Device names match.

     

    In Control Panel > Directories > Libraries, your personal libraries

    paths should probably be listed first and concentrating on not naming

    libraries the same as Eagle does is a good idea.

     

    HTH

    Warren

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • celestine
    0 celestine over 6 years ago in reply to autodeskguest

    Thank you (again) Chuck and also Warren.

    I am slowly figuring this out.

    Also, I am taking what both of you have said (Cut-and-paste) and putting it my own  Eagle "Help File", separate from any Autodesk/Eagle website.

    (I don't trust any website not to change//archive/purge older posts, pics etc...."Once burned, twice shy.") 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 6 years ago in reply to dukepro

    On 17/07/2020 2:07 am, Chuck Huber wrote:

     

    For example: suppose Eagle's rcl.lbr contains a resistor, and your

    personal library does to.  When your design is updated from your

    personal library, only resistors that were sourced from your personal

    library will be affected.  The resistors in your design that were

    sourced from Eagle's rcl.lbr will not be affected.

     

    HI Chuck, this is not the full story if you don't specify the library

    and use "Update all"

     

    In this case a design will be updated from the first library Eagle finds

    with the correct library name with a matching device within it.

     

    So, when you set up Control Panel > Directories > Libraries, the order

    of the library paths is the order Eagle uses and as soon as it gets a

    Library/Device match it updates the design using that device because the

    library/Device names match.

     

    In Control Panel > Directories > Libraries, your personal libraries

    paths should probably be listed first and concentrating on not naming

    libraries the same as Eagle does is a good idea.

     

    HTH

    Warren

     

    --

    ... use NNTP://news.cadsoft.de and a functional news reader like

    Thunderbird!

     

    --

    This email has been checked for viruses by Avast antivirus software.

    https://www.avast.com/antivirus

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dukepro
    0 dukepro over 6 years ago in reply to celestine

    Patricia,

     

    Other things to note.

     

    A copy of every symbol, package, and device used in a project is kept in

    both the schematic and board files.  Also maintained in the schematic

    and board files is the source library of each device.  The purpose of

    this is reproducibility.  Years from now, you should be able to open the

    project and have everything exactly as you had left it, regardless of

    how extensive the changes to any of the libraries from which parts were

    sourced.  You can witness this by opening the .sch file with a plain

    text editor like vi, emacs, or (God forgive) ed.  I'm sure Windoze has

    an equivalent (Notepad?), but I don't trust MS to not embed special

    characters within what otherwise should be plain text.  Maybe they

    haven't lost all sanity.  Maybe they have.

     

    Reproducibility is nice.  And it's necessary.  However, it is also

    necessary from time to time to update existing elements of a design to

    those contained within a library.  This is where the Library Update

    comes in.  A bit backwards in the nomenclature, this does /not/ refer to

    updating a library.  Instead it refers to updating a design /from/ a

    library.  In this process, Eagle will scan through all the devices in

    your design, searching for devices that are sourced from the library

    from which you're updating.  The symbols and packages in your design are

    updated from their counterparts in the library.

     

    For example: suppose Eagle's rcl.lbr contains a resistor, and your

    personal library does to.  When your design is updated from your

    personal library, only resistors that were sourced from your personal

    library will be affected.  The resistors in your design that were

    sourced from Eagle's rcl.lbr will not be affected.

     

    Also bear in mind that Eagle will occasionally update the libraries in

    their distribution.  It is a good practice to copy devices that you use

    from the distribution libraries into your own personal library.  In this

    manner, /you/ control what gets changed in your design.  Thus, arbitrary

    changes in Eagle's libraries do not generate problems years down the road.

     

    The Library Update function can be accessed by clicking on

    Library->Update and choosing the library from which you wish to update. 

    It can also be access by typing UPDATE into Eagle's command text box,

    optionally followed by the name of the library to update.

     

    HTH,

        - Chuck

     

     

    On 7/16/20 06:30, Patricia Hann wrote:

    Thank you Chuck.....I had kind of figured it out before you answered, but, as you say, things are never simple.

    And you clarified the order of how to access a library in a way that is helpful for me to remember it.

    I did not know that if I removed a device from the library it does not affect the device if it is already "in use"   schematic or layout.  Good to know.

      I know I will have other questions as I learn Eagle,... this is probably only the first of many questions. but I am determined to learn it.

    THanks again

     

     

     

    Attachments:
    72532.att1.html.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • celestine
    0 celestine over 6 years ago in reply to dukepro

    Thank you Chuck.....I had kind of figured it out before you answered, but, as you say, things are never simple.

    And you clarified the order of how to access a library in a way that is helpful for me to remember it.

    I did not know that if I removed a device from the library it does not affect the device if it is already "in use"   schematic or layout.  Good to know.

    I know I will have other questions as I [attempt to!] learn Eagle,... this is probably only the first of many questions. but I am determined to learn it.

    THanks again      

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 6 years ago in reply to dukepro

    On 14/07/2020 13:36, Chuck Huber wrote:

     

    Caveat emptor: This advice applies to Eagle v7.7.

     

    ... back when things were simple.

     

    The recent AutoDesk versions have a "library manager" which makes all of

    this choosing of libraries more "modern". To my mind, that translates as

    "harder and less intuitive" but then I'm a dinosaur who's gone back to

    V7.7 because I prefer it.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dukepro
    0 dukepro over 6 years ago in reply to celestine

    Patricia,

     

    The libraries available are listed in the control panel.  As you

    mentioned, your library is listed there.  From that presence, your

    library path is correct and does not need to be changed for this purpose.

     

    Every design uses a specific enumerated set of libraries.  There's no

    reason for Eagle to load /all/ of the libraries when only a few will be

    used.  The USE command will open a dialog box and allows you to pick

    which libraries will be included in the current project.  I suspect that

    your custom library is not in that list.  To get to this, you can type

    "USE" into the command text box, or you can click on Library->Use.

     

    To reverse this process (i.e. to un-use a library), use the ADD

    command.  This is the same command used to add components to a

    schematic.  The dialog box provides the opportunity to select a library

    and "Un-Use" it, thus removing it from the list of libraries used by the

    project.  To do this, you can type "ADD" into the command text box, or

    you can click on Edit->Add.

     

    It is pertinent to note that removing a library from the list does NOT

    remove the devices already one the schematic that were sourced from that

    library.  Un-using the library merely takes it off the list of libraries

    from which components can be /added/ to a schematic.

     

    Caveat emptor: This advice applies to Eagle v7.7.

     

    Best regards,

        - Chuck

     

     

     

    On 7/14/20 01:43, Patricia Hann wrote:

    Im using Windows 10

    Eagle 9.6.2

     

    As for the rest of what you said to do....really I have no idea what you telling me to do.

    Shouldn't I be able to click on "libraries" tab at the top of the schematic page and just open the folder I need?

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/294065

     

     

    Attachments:
    0247.att1.html.zip