Hi,
when using large traces their ends are rounded. This is a problem in
some smd situations.
For example, see this picture:
http://www.students.tut.fi/~kontkant/cont/ele-a3977/005-intro/telok3.png
Note the large traces at both high corners of the smd chip in the middle
of the pcb. The guy was able to connect them to the pad without. If I do
the same the edge will be rounded and this leads to shorts the nearest pad.
How to have sharp edges at the ends of a trace?
Thanks
Marco / iw2nzm