EAGLE User Support (English) Traces with no round egde
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
  • Replies 6 replies
  • Subscribers 179 subscribers
  • Views 532 views
  • Users 0 members are here
Related

Traces with no round egde

autodeskguest
autodeskguest over 17 years ago

Hi,

 

when using large traces their ends are rounded. This is a problem in

some smd situations.

 

For example, see this picture:

 

http://www.students.tut.fi/~kontkant/cont/ele-a3977/005-intro/telok3.png

 

Note the large traces at both high corners of the smd chip in the middle

of the pcb. The guy was able to connect them to the pad without. If I do

the same the edge will be rounded and this leads to shorts the nearest pad.

 

How to have sharp edges at the ends of a trace?

 

Thanks

Marco / iw2nzm

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    On Fri, 02 May 2008 06:16:07 +0200, Paul Romanyszyn 

    <pgr@arcelectronicsinc.com> wrote:

     

    For any traces larger then 16 mil I use named polygon's.

    see http://arcelectronicsinc.com/testinfo/eca-320polygons.png

     

    How did you do this print? Not manually I hope?

     

     

    Wouter

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    On Fri, 02 May 2008 06:16:07 +0200, Paul Romanyszyn 

    <pgr@arcelectronicsinc.com> wrote:

     

    For any traces larger then 16 mil I use named polygon's.

    see http://arcelectronicsinc.com/testinfo/eca-320polygons.png

     

    How did you do this print? Not manually I hope?

     

     

    Wouter