EAGLE User Support (English) polygon circle
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
  • Replies 1 reply
  • Subscribers 178 subscribers
  • Views 319 views
  • Users 0 members are here
Related

polygon circle

tcbob
tcbob over 17 years ago

hello,

 

I need to create a 1 inch polygon circle, what is the easiest way to do

that?

 

thanks,

 

 

 

  • Sign in to reply
  • Cancel
  • Richard_H
    Richard_H over 17 years ago

    Bob schrieb:

    hello,

     

    I need to create a 1 inch polygon circle, what is the easiest way to do

    that?

     

    thanks,

     

    Maybe a bit unconventional, but quick:

     

    GRID  0.5 inch;

    SET WIRE_BEND 2;

     

    Draw a POLYGON like this one:

     

       /\

       \/   (should look like a square, rotated by 45°) 5 mouse clicks

     

    Now use MOVE and click the upper vertex and move it down,

    looks like this

        _

       \ /  (it's a triangle)  2 mouse clicks

     

    Now activate MOVE, press Ctrl and click the horizontal line

    in the middle and move it back upwards. A semicircle appears.

    again 2 mouse clicks

     

    Do the same for the bottom part.

     

    So you draw a circle polygon with a diameter of 1 inch.

     

    Without calculating anything.  image

     

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm