EAGLE User Support (English) All pins off grid, pads move when viewing gerbers
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
  • Replies 3 replies
  • Subscribers 178 subscribers
  • Views 359 views
  • Users 0 members are here
Related

All pins off grid, pads move when viewing gerbers

autodeskguest
autodeskguest over 17 years ago

Hi, I'm new to eagle. Designing a small two-layer relay board.

 

When I place the relays from the library, the outer packages "snap" to the

grid, which I have set at .025. However, apparently all the pins are off

grid and the DRC gives me about 20 errors. Is this anything to worry about?

Can I/should I make the PINS snap to the grid instead of the package

outline, and if so, how do I do this?

 

More troubling, when I view the Gerbers with a free viewer (Viewmate 10)

some of the pads are displaced between the two layers... in one case, they

are "next to" each other instead of being "on top of" each other as they

should be.  Is this related to all the pins being off grid?

 

Thanks

 

--eric g

 

 

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Eric Griswold wrote:

    Hi, I'm new to eagle. Designing a small two-layer relay board.

     

    When I place the relays from the library, the outer packages "snap"

    to the grid, which I have set at .025. However, apparently all the

    pins are off grid and the DRC gives me about 20 errors. Is this

    anything to worry about? Can I/should I make the PINS snap to the

    grid instead of the package outline, and if so, how do I do this?

     

    Your pads don't need to be on-grid.  For tidy looking routing, start your

    traces at these off-grid pads and route them to an on-grid point.

     

    More troubling, when I view the Gerbers with a free viewer (Viewmate

    10) some of the pads are displaced between the two layers... in one

    case, they are "next to" each other instead of being "on top of" each

    other as they should be.  Is this related to all the pins being off

    grid?

     

    I don't know what is wrong there.  Sometimes Gerber formats get confused.

    It's best to use the RS274X format, as produced by the ger274x.cam CAM file.

    I use GC-Prevue to peruse the Gerbers produced by Eagle.

     

    --

    Bert Menkveld

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Eric Griswold schrieb:

     

    When I place the relays from the library, the outer packages "snap" to the

    grid, which I have set at .025. However, apparently all the pins are off

    grid and the DRC gives me about 20 errors. Is this anything to worry about?

    Can I/should I make the PINS snap to the grid instead of the package

    outline, and if so, how do I do this?

     

    As Bert already mentioned, the pads don't need to be on-grid. Many parts

    (especially those with "metric" packages) have off-grid pads, regardless

    of the grid you use for routing.

    Just take care to always start routing at the off-grid pad and end

    somewhere on grid.

     

    More troubling, when I view the Gerbers with a free viewer (Viewmate 10)

    some of the pads are displaced between the two layers... in one case, they

    are "next to" each other instead of being "on top of" each other as they

    should be.  Is this related to all the pins being off grid?

     

    Simply take a /working/ gerber viewer. I have heard of many (more or

    less serious) problems with Viewmate. Personally, I prefer GCprevue (in

    fact an older version...).

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Eric Griswold wrote:

    Hi, I'm new to eagle. Designing a small two-layer relay board.

     

    When I place the relays from the library, the outer packages "snap" to the

    grid, which I have set at .025. However, apparently all the pins are off

    grid and the DRC gives me about 20 errors. Is this anything to worry about?

    Can I/should I make the PINS snap to the grid instead of the package

    outline, and if so, how do I do this?

     

     

    If the pins would lie on the grid then it is better practice to line them up

    that way when you make the package rather than the package outline on grid.

     

    However off grid DRC errors are not something to worry about unless you have

    some special conditions. I never have that option checked in the DRC (or angle)

     

    cheers

     

    David