EAGLE User Support (English) All pins off grid, pads move when viewing gerbers
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
  • Replies 3 replies
  • Subscribers 178 subscribers
  • Views 363 views
  • Users 0 members are here
Related

All pins off grid, pads move when viewing gerbers

autodeskguest
autodeskguest over 17 years ago

Hi, I'm new to eagle. Designing a small two-layer relay board.

 

When I place the relays from the library, the outer packages "snap" to the

grid, which I have set at .025. However, apparently all the pins are off

grid and the DRC gives me about 20 errors. Is this anything to worry about?

Can I/should I make the PINS snap to the grid instead of the package

outline, and if so, how do I do this?

 

More troubling, when I view the Gerbers with a free viewer (Viewmate 10)

some of the pads are displaced between the two layers... in one case, they

are "next to" each other instead of being "on top of" each other as they

should be.  Is this related to all the pins being off grid?

 

Thanks

 

--eric g

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    Eric Griswold wrote:

    Hi, I'm new to eagle. Designing a small two-layer relay board.

     

    When I place the relays from the library, the outer packages "snap" to the

    grid, which I have set at .025. However, apparently all the pins are off

    grid and the DRC gives me about 20 errors. Is this anything to worry about?

    Can I/should I make the PINS snap to the grid instead of the package

    outline, and if so, how do I do this?

     

     

    If the pins would lie on the grid then it is better practice to line them up

    that way when you make the package rather than the package outline on grid.

     

    However off grid DRC errors are not something to worry about unless you have

    some special conditions. I never have that option checked in the DRC (or angle)

     

    cheers

     

    David

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    Eric Griswold wrote:

    Hi, I'm new to eagle. Designing a small two-layer relay board.

     

    When I place the relays from the library, the outer packages "snap" to the

    grid, which I have set at .025. However, apparently all the pins are off

    grid and the DRC gives me about 20 errors. Is this anything to worry about?

    Can I/should I make the PINS snap to the grid instead of the package

    outline, and if so, how do I do this?

     

     

    If the pins would lie on the grid then it is better practice to line them up

    that way when you make the package rather than the package outline on grid.

     

    However off grid DRC errors are not something to worry about unless you have

    some special conditions. I never have that option checked in the DRC (or angle)

     

    cheers

     

    David