EAGLE User Support (English) Eagle 5.0 linux beginner user
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
  • Replies 3 replies
  • Subscribers 178 subscribers
  • Views 421 views
  • Users 0 members are here
Related

Eagle 5.0 linux beginner user

autodeskguest
autodeskguest over 17 years ago

Hello everyone,

i am glad to see even version 5 is available with the freeware license

for the hobbyst, i started using eagle in linux from version 4 but only

version 5 works PERFECTLY.

 

Since i am a novice i incurred in some annoying problems which could be

easily fixed by someone more expert:

 

1) once i autoroute the circuit i am unable to rotate or move the

components, to do so i have to type 'namecomponent' in the box that

appears when clicking on move component, otherwise is not possible to

select anything that is not a route.

 

2) i am trying to make a double side circuit for the first time, it does

work and is convenient, but i am unable to make a clean picture for the

photoetching of the circuit: if i select for example to show ONLY top

layer, i still see the pads ALSO of the bottom layer...how can i fix it?

till now i can only remove ALL the pads or not...if i try to print only

the bottom, well the pads of the top also show there!!!

 

That's all! thank you very much

 

Agostino

 

 

  • Sign in to reply
  • Cancel
  • Richard_H
    Richard_H over 17 years ago

    Agostino Nevermore schrieb:

    Hello everyone,

    i am glad to see even version 5 is available with the freeware license

    for the hobbyst, i started using eagle in linux from version 4 but only

    version 5 works PERFECTLY.

     

    Since i am a novice i incurred in some annoying problems which could be

    easily fixed by someone more expert:

     

    1) once i autoroute the circuit i am unable to rotate or move the

    components, to do so i have to type 'namecomponent' in the box that

    appears when clicking on move component, otherwise is not possible to

    select anything that is not a route.

     

    Please chick if the layers tOrigin and bOrigin are visible.

    Otherwise you can't select components.

     

     

    2) i am trying to make a double side circuit for the first time, it does

    work and is convenient, but i am unable to make a clean picture for the

    photoetching of the circuit: if i select for example to show ONLY top

    layer, i still see the pads ALSO of the bottom layer...how can i fix it?

    till now i can only remove ALL the pads or not...if i try to print only

    the bottom, well the pads of the top also show there!!!

     

     

    Pads go through all layers. They are visible on top and on bottom.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Agostino Nevermore wrote:

    Hello everyone,

    i am glad to see even version 5 is available with the freeware license

    for the hobbyst, i started using eagle in linux from version 4 but only

    version 5 works PERFECTLY.

     

    Since i am a novice i incurred in some annoying problems which could be

    easily fixed by someone more expert:

     

    1) once i autoroute the circuit i am unable to rotate or move the

    components, to do so i have to type 'namecomponent' in the box that

    appears when clicking on move component, otherwise is not possible to

    select anything that is not a route.

     

    As a novice now is the time to brush up on your manual routing skills.

    Learn about current mirroring and numerous other important issues.  If doing

    4 layers of more then consider autorouting.

     

     

    2) i am trying to make a double side circuit for the first time, it does

    work and is convenient, but i am unable to make a clean picture for the

    photoetching of the circuit: if i select for example to show ONLY top

    layer, i still see the pads ALSO of the bottom layer...how can i fix it?

    till now i can only remove ALL the pads or not...if i try to print only

    the bottom, well the pads of the top also show there!!!

     

     

    Are you talking about through hole pads or SMT pads?  Through hole

    components will of course have pads on both sides of the board.

     

     

    If you are seeing some artefacts of SMT pads then check your displayed layers.

     

    cheers

     

    David

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Il Thu, 05 Jun 2008 11:09:53 +0100, David Moodie ha scritto:

     

    Thanks everyone

    i am not able to manually route stuffs, but i am already able to use

    mirroring and other features to make easier for the autorouter..

    Now the real problem is the CRAZY price of the photoetching boards!!!

    Thanks

    Agostino