EAGLE User Support (English) Eagle 5.0 linux beginner user
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
  • Replies 3 replies
  • Subscribers 178 subscribers
  • Views 423 views
  • Users 0 members are here
Related

Eagle 5.0 linux beginner user

autodeskguest
autodeskguest over 17 years ago

Hello everyone,

i am glad to see even version 5 is available with the freeware license

for the hobbyst, i started using eagle in linux from version 4 but only

version 5 works PERFECTLY.

 

Since i am a novice i incurred in some annoying problems which could be

easily fixed by someone more expert:

 

1) once i autoroute the circuit i am unable to rotate or move the

components, to do so i have to type 'namecomponent' in the box that

appears when clicking on move component, otherwise is not possible to

select anything that is not a route.

 

2) i am trying to make a double side circuit for the first time, it does

work and is convenient, but i am unable to make a clean picture for the

photoetching of the circuit: if i select for example to show ONLY top

layer, i still see the pads ALSO of the bottom layer...how can i fix it?

till now i can only remove ALL the pads or not...if i try to print only

the bottom, well the pads of the top also show there!!!

 

That's all! thank you very much

 

Agostino

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    Il Thu, 05 Jun 2008 11:09:53 +0100, David Moodie ha scritto:

     

    Thanks everyone

    i am not able to manually route stuffs, but i am already able to use

    mirroring and other features to make easier for the autorouter..

    Now the real problem is the CRAZY price of the photoetching boards!!!

    Thanks

    Agostino

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    Il Thu, 05 Jun 2008 11:09:53 +0100, David Moodie ha scritto:

     

    Thanks everyone

    i am not able to manually route stuffs, but i am already able to use

    mirroring and other features to make easier for the autorouter..

    Now the real problem is the CRAZY price of the photoetching boards!!!

    Thanks

    Agostino