EAGLE User Support (English) Capacitance sensing pads
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
  • Replies 5 replies
  • Subscribers 177 subscribers
  • Views 387 views
  • Users 0 members are here
Related

Capacitance sensing pads

autodeskguest
autodeskguest over 17 years ago

I'm trying to make some symbols to use as capacitive sensing buttons for use

with a Cypress PSoC Capsense chip. The Cypress application note (AN2292)

says to fill ground around the pads. I can't figure out how to create a

buffer area to keep the polygon from filling right over the pads. Any ideas?

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

     

    If using two polygons then the inner polygon needs to have a lower rank

    than the outer. See Help polygon, where there are a few lines on Rank.

    You do not need to take special care about drawing the outer polygon.

    The isolation will be set depending upon the isolation value of the

    polygons, the higher value being used.

     

    cheers

     

    David

     

     

     

    LGR wrote:

    > I guess I wasn't clear. The symbol consists of a through-hole pad

    (which is

    > what the device connects to on the bottom layer), and a polygon

    around it.

    > The polygon has to be made in the top layer only, because that's

    where the

    > touch sensing happens. I can't make it with layer 17, because that would

    > create polygons on both top and bottom. For the buttons, I suppose I

    could

    > distort an SMD, but I also need to create W-shaped elements for the

    > "slider". If you're curious, here's the application note:

    >

    >

    http://download.cypress.com.edgesuite.net/design_resources/application_notes/contents/capacitance_sensing___layout_guidelines_for_psoc_capsense___an2292_12.pdf

     

    I'm not sure that you read his post correctly, he's just saying to

    change the rank of the key polygon to be lower than the ground

    polygon. Not the layer or anything else. More information can be found

    by typing "help polygon" in the command area of the editor like David

    mentioned.

     

    Edward

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

     

    If using two polygons then the inner polygon needs to have a lower rank

    than the outer. See Help polygon, where there are a few lines on Rank.

    You do not need to take special care about drawing the outer polygon.

    The isolation will be set depending upon the isolation value of the

    polygons, the higher value being used.

     

    cheers

     

    David

     

     

     

    LGR wrote:

    > I guess I wasn't clear. The symbol consists of a through-hole pad

    (which is

    > what the device connects to on the bottom layer), and a polygon

    around it.

    > The polygon has to be made in the top layer only, because that's

    where the

    > touch sensing happens. I can't make it with layer 17, because that would

    > create polygons on both top and bottom. For the buttons, I suppose I

    could

    > distort an SMD, but I also need to create W-shaped elements for the

    > "slider". If you're curious, here's the application note:

    >

    >

    http://download.cypress.com.edgesuite.net/design_resources/application_notes/contents/capacitance_sensing___layout_guidelines_for_psoc_capsense___an2292_12.pdf

     

    I'm not sure that you read his post correctly, he's just saying to

    change the rank of the key polygon to be lower than the ground

    polygon. Not the layer or anything else. More information can be found

    by typing "help polygon" in the command area of the editor like David

    mentioned.

     

    Edward