EAGLE User Support (English) Capacitance sensing pads
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
  • Replies 5 replies
  • Subscribers 177 subscribers
  • Views 385 views
  • Users 0 members are here
Related

Capacitance sensing pads

autodeskguest
autodeskguest over 17 years ago

I'm trying to make some symbols to use as capacitive sensing buttons for use

with a Cypress PSoC Capsense chip. The Cypress application note (AN2292)

says to fill ground around the pads. I can't figure out how to create a

buffer area to keep the polygon from filling right over the pads. Any ideas?

 

 

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    LGR wrote:

    I'm trying to make some symbols to use as capacitive sensing buttons for use

    with a Cypress PSoC Capsense chip. The Cypress application note (AN2292)

    says to fill ground around the pads. I can't figure out how to create a

    buffer area to keep the polygon from filling right over the pads. Any ideas?

     

     

    If the pads are made using SMD pads or through-hole pads, any polygon

    drawn around them but named differently from the signals on the pads

    will automatically have an isolation space around the pads.

    If you draw the touch pads using polygons, you will just have to be

    careful how you draw the ground polygon outline so an isolation space is

    left.

    John G.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    John Giddy wrote:

    LGR wrote:

    I'm trying to make some symbols to use as capacitive sensing buttons

    for use with a Cypress PSoC Capsense chip. The Cypress application

    note (AN2292) says to fill ground around the pads. I can't figure out

    how to create a buffer area to keep the polygon from filling right

    over the pads. Any ideas?

     

    If the pads are made using SMD pads or through-hole pads, any polygon

    drawn around them but named differently from the signals on the pads

    will automatically have an isolation space around the pads.

    If you draw the touch pads using polygons, you will just have to be

    careful how you draw the ground polygon outline so an isolation space is

    left.

    John G.

     

    If using two polygons then the inner polygon needs to have a lower rank than

    the outer. See Help polygon, where there are a few lines on Rank.

      You do not need to take special care about drawing the outer polygon.  The

    isolation will be set depending upon the isolation value of the polygons,

    the higher value being used.

     

    cheers

     

    David

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    I guess I wasn't clear. The symbol consists of a through-hole pad (which is

    what the device connects to on the bottom layer), and a polygon around it.

    The polygon has to be made in the top layer only, because that's where the

    touch sensing happens. I can't make it with layer 17, because that would

    create polygons on both top and bottom. For the buttons, I suppose I could

    distort an SMD, but I also need to create W-shaped elements for the

    "slider". If you're curious, here's the application note:

     

    http://download.cypress.com.edgesuite.net/design_resources/application_notes/contents/capacitance_sensing___layout_guidelines_for_psoc_capsense___an2292_12.pdf

     

    "David Moodie" <dgmoodie@onetel.com.cut_this_off> wrote in message

    news:g2qoqd$phh$1@cheetah.cadsoft.de...

    John Giddy wrote:

    LGR wrote:

    I'm trying to make some symbols to use as capacitive sensing buttons for

    use with a Cypress PSoC Capsense chip. The Cypress application note

    (AN2292) says to fill ground around the pads. I can't figure out how to

    create a buffer area to keep the polygon from filling right over the

    pads. Any ideas?

     

    If the pads are made using SMD pads or through-hole pads, any polygon

    drawn around them but named differently from the signals on the pads will

    automatically have an isolation space around the pads.

    If you draw the touch pads using polygons, you will just have to be

    careful how you draw the ground polygon outline so an isolation space is

    left.

    John G.

     

    If using two polygons then the inner polygon needs to have a lower rank

    than the outer. See Help polygon, where there are a few lines on Rank.

    You do not need to take special care about drawing the outer polygon.

    The isolation will be set depending upon the isolation value of the

    polygons, the higher value being used.

     

    cheers

     

    David

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

     

    If using two polygons then the inner polygon needs to have a lower rank

    than the outer. See Help polygon, where there are a few lines on Rank.

    You do not need to take special care about drawing the outer polygon.

    The isolation will be set depending upon the isolation value of the

    polygons, the higher value being used.

     

    cheers

     

    David

     

     

     

    LGR wrote:

    > I guess I wasn't clear. The symbol consists of a through-hole pad

    (which is

    > what the device connects to on the bottom layer), and a polygon

    around it.

    > The polygon has to be made in the top layer only, because that's

    where the

    > touch sensing happens. I can't make it with layer 17, because that would

    > create polygons on both top and bottom. For the buttons, I suppose I

    could

    > distort an SMD, but I also need to create W-shaped elements for the

    > "slider". If you're curious, here's the application note:

    >

    >

    http://download.cypress.com.edgesuite.net/design_resources/application_notes/contents/capacitance_sensing___layout_guidelines_for_psoc_capsense___an2292_12.pdf

     

    I'm not sure that you read his post correctly, he's just saying to

    change the rank of the key polygon to be lower than the ground

    polygon. Not the layer or anything else. More information can be found

    by typing "help polygon" in the command area of the editor like David

    mentioned.

     

    Edward

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    LGR wrote:

    I guess I wasn't clear. The symbol consists of a through-hole pad (which is

    what the device connects to on the bottom layer), and a polygon around it.

    The polygon has to be made in the top layer only, because that's where the

    touch sensing happens. I can't make it with layer 17, because that would

    create polygons on both top and bottom. For the buttons, I suppose I could

    distort an SMD, but I also need to create W-shaped elements for the

    "slider". If you're curious, here's the application note:

     

    http://download.cypress.com.edgesuite.net/design_resources/application_notes/contents/capacitance_sensing___layout_guidelines_for_psoc_capsense___an2292_12.pdf

     

     

    Avoid top posting in newsgroups- the threads don't make sense that way.

     

     

     

    OK I guess it wasn't too clear to me. But here's my second guess.  You

    actually want to make a package in the library?  The libraries do not handle

    polygons well.

     

    My first guess was that you were just going to draw this straight on the

    PCB, which is where polygons of different rank make drawing this relatively

    straightforward.  If you want more than one pad, then use copy-cut and paste

    for the polygons

     

     

    cheers

     

    David