Hi,
Is there anyway to change the height above the board of the PCB traces and pads in EagleCad?
Hi,
Is there anyway to change the height above the board of the PCB traces and pads in EagleCad?
On 08/11/2010 11:50 AM, Olin Lathrop wrote:
Matt Collinge wrote on Wed, 11 August 2010 11:21
>> Is there anyway to change the height above the board of the PCB traces
>> and pads in EagleCad?
No, that is something you specify to the board house separately from the
gerber files. Generally you get "1 ounce" copper thickness (I think that
is the weight of copper per square foot, but can be translated to a
explicit thickness in um, mil, or whatever). You pay more for thicker
copper, like 2 ounce and 4 ounce. 4 ounce is pretty thick. If you need
more than that, you probably have to rethink what you're doing, use wider
traces, run bus bars, etc.
Important to note also is that the copper thickness is specified on a
per-layer basis. That is, each layer must be of uniform thickness. You
can not have particular traces thicker than others on the same layer.
I have had several instances where I needed a high current trace (single
impulse of 300+ amps) but could not afford the area that it would
occupy. To accommodate this, I place a wire on the mask layer that was
directly above the copper layer, and later coated the copper trace with
solder.
Hope this helps.
Enjoy,
- Chuck
On 08/11/2010 11:50 AM, Olin Lathrop wrote:
Matt Collinge wrote on Wed, 11 August 2010 11:21
>> Is there anyway to change the height above the board of the PCB traces
>> and pads in EagleCad?
No, that is something you specify to the board house separately from the
gerber files. Generally you get "1 ounce" copper thickness (I think that
is the weight of copper per square foot, but can be translated to a
explicit thickness in um, mil, or whatever). You pay more for thicker
copper, like 2 ounce and 4 ounce. 4 ounce is pretty thick. If you need
more than that, you probably have to rethink what you're doing, use wider
traces, run bus bars, etc.
Important to note also is that the copper thickness is specified on a
per-layer basis. That is, each layer must be of uniform thickness. You
can not have particular traces thicker than others on the same layer.
I have had several instances where I needed a high current trace (single
impulse of 300+ amps) but could not afford the area that it would
occupy. To accommodate this, I place a wire on the mask layer that was
directly above the copper layer, and later coated the copper trace with
solder.
Hope this helps.
Enjoy,
- Chuck