EAGLE User Support (English) Libray 4.1 <=> 5.1
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
  • Replies 4 replies
  • Subscribers 178 subscribers
  • Views 239 views
  • Users 0 members are here
Related

Libray 4.1 <=> 5.1

autodeskguest
autodeskguest over 17 years ago

I just got a library created in version 4.1.

What i see now in the schematics in version 5.1 is the text P$2 at a

terminal from the device. When used in version 4.1 it doenst show.

 

Must i do something to use a library created in 4.1 to be used in 5.1

 

Harry

 

 

 

 

 

 

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

     

    "Richard Hammerl" <ric@cadsoft.de> wrote in message

    news:g4kk0m$9rf$1@cheetah.cadsoft.de...

    Harry H. Arends schrieb:

    I just got a library created in version 4.1.

    What i see now in the schematics in version 5.1 is the text P$2 at a

    terminal from the device. When used in version 4.1 it doenst show.

     

    Must i do something to use a library created in 4.1 to be used in 5.1

     

    Harry

     

    No, you dont' have to do something special. Simply use it.

     

    The texts that are shown at the pin are defined in the Symbol

    with the CHANGE VISIBLE command. I can't imagine that this

    setting changes while updating from 4.1 to 5.

    Could you please verify the "visible" setting in the 4.1 library?

     

    Richard,

     

    I created the device for Harry in version 4.1

     

    In the symbol the "Visible" parameter is indeed set to "Both" because I

    renamed the pins as P$1 => Vs, P$2 => GND and P$3 => Q and the package pins

    are named 1, 2 and 3. As you can see from the attachment, both pin and pad

    names are correct when I insert it in a schematic in version 4.1

     

    In version 5.1 however, the pad names appear as P$2, P$3 and P$4 as you can

    see in the pic that Harry sent (BTW, I wonder why not P$1, P$2 & P$3?).

    Looks to me as there is a potential conversion issue when using library

    symbols created in 4.1 in version 5.1

     

    Robert

     

     

     

     

     

     

    Attachments:
    image
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 17 years ago in reply to autodeskguest

    Robert schrieb:

     

    Richard,

     

    I created the device for Harry in version 4.1

     

    In the symbol the "Visible" parameter is indeed set to "Both" because I

    renamed the pins as P$1 => Vs, P$2 => GND and P$3 => Q and the package pins

    are named 1, 2 and 3. As you can see from the attachment, both pin and pad

    names are correct when I insert it in a schematic in version 4.1

     

    In version 5.1 however, the pad names appear as P$2, P$3 and P$4 as you can

    see in the pic that Harry sent (BTW, I wonder why not P$1, P$2 & P$3?).

    Looks to me as there is a potential conversion issue when using library

    symbols created in 4.1 in version 5.1

     

    Robert

     

    Can you please send me the library file of version 4.1, so

    I can try to reproduce this?

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 17 years ago in reply to autodeskguest

    Robert schrieb:

     

    Richard,

     

    I created the device for Harry in version 4.1

     

    In the symbol the "Visible" parameter is indeed set to "Both" because I

    renamed the pins as P$1 => Vs, P$2 => GND and P$3 => Q and the package pins

    are named 1, 2 and 3. As you can see from the attachment, both pin and pad

    names are correct when I insert it in a schematic in version 4.1

     

    In version 5.1 however, the pad names appear as P$2, P$3 and P$4 as you can

    see in the pic that Harry sent (BTW, I wonder why not P$1, P$2 & P$3?).

    Looks to me as there is a potential conversion issue when using library

    symbols created in 4.1 in version 5.1

     

    Robert

     

    Can you please send me the library file of version 4.1, so

    I can try to reproduce this?

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm