Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Mac 5.11 (and 5.10) frequently hangs
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 187 subscribers
  • Views 531 views
  • Users 0 members are here
  • schematic
  • mac
Related

Mac 5.11 (and 5.10) frequently hangs

e14 Contributor
e14 Contributor over 15 years ago

Hi!

 

I've just started using Eagle on Mac (10.6.7, Macbook Air with 2 Gb ram, 1.4 GHz Core 2 Duo) and it frequently hangs in the library

window (add command). I have to kill the process. I've waited for 30 minutes which seems "long enough" for a library lookup:-)

 

One that makes it hang every time is "resistor"; I tried downloading the updated resistor_3rdPin_v20.lbr but I get same result.

For these two, I cannot even click on the arrow to expand the library view with the components. (Naturally, I can do so on all the other

libraries I've tried, including the other resistor-libraries.)

 

Any hints?

 

I'm going to try this on a Windows machine to see if that works, but that's not really a solution for me.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    I followed the other response and did "use -*" and then I tried opening

    the resistor.lbr library.

    Works fine as far as I can tell.

     

    However, when I put it back and did "use resistor.lbr" followed by

    "add", eagle hangs as soon

    as I click on resistor.lbr. It even hangs when I do "add" and click on Cancel.

     

    However, I can do "add r-eu_r0805" and add devices to my schematic.

     

    Something is wrong in the library viewer.

     

    Anyway, I have none of these issues in the in the windows version.

     

    Is there anything I can send you to help you pin this down?

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    I followed the other response and did "use -*" and then I tried opening

    the resistor.lbr library.

    Works fine as far as I can tell.

     

    However, when I put it back and did "use resistor.lbr" followed by

    "add", eagle hangs as soon

    as I click on resistor.lbr. It even hangs when I do "add" and click on Cancel.

     

    However, I can do "add r-eu_r0805" and add devices to my schematic.

     

    Something is wrong in the library viewer.

     

    Anyway, I have none of these issues in the in the windows version.

     

    Is there anything I can send you to help you pin this down?

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Richard_H
    0 Richard_H over 15 years ago in reply to e14 Contributor

    Am 01.06.2011 22:42, schrieb Torbjörn Lindh:

    I followed the other response and did "use -*" and then I tried opening

    the resistor.lbr library.

    Works fine as far as I can tell.

     

    However, when I put it back and did "use resistor.lbr" followed by

    "add", eagle hangs as soon

    as I click on resistor.lbr. It even hangs when I do "add" and click on

    Cancel.

     

    However, I can do "add r-eu_r0805" and add devices to my schematic.

     

    Something is wrong in the library viewer.

     

    Anyway, I have none of these issues in the in the windows version.

     

    Is there anything I can send you to help you pin this down?

     

     

    Could you please send me the library file that makes problems and

    the configuration file  .eaglerc  which should be in your home

    directory?

    Send it to the email address mentioned in the signature.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm