Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Eagle Standar 8 Layer StackUp
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 180 subscribers
  • Views 1358 views
  • Users 0 members are here
  • eagle
  • stackup
  • layers
Related

Eagle Standar 8 Layer StackUp

Former Member
Former Member over 14 years ago

Hi All,

 

Im trying to create an 8 Layer PCB stackup I want to follow the best practices and I fond this site: http://www.hottconsultants.com along with many other that say that my 8 layer board stackup should be make like this (for better EMC and signal integrity)

 

~~~~~~~~~~~~~~~  Mounting Pads/Low Freq. Signals

:::::::::::::::  Prepreg

+++++++++++++++  Pwr.

===============  FR4 Core
---------------  Gnd.
:::::::::::::::  Prepreg
~~~~~~~~~~~~~~~  High Freq. Signals
===============  FR4 Core
~~~~~~~~~~~~~~~  High Freq. Signals
:::::::::::::::  Prepreg
---------------  Gnd.
===============  FR4 Core
+++++++++++++++  Pwr.
:::::::::::::::  Prepreg
~~~~~~~~~~~~~~~  Low Freq. Signals/Test Pads

 

I've never worked with eagle with so many layers, and never even bother with blind and burried vias.

I need some help to define this stackup in eagle and also to create the throu, burried and blind vias to connect the layers.

 

This is the very basic stackup I've with no vias image

image

 

Thanks in advance.

 

Ben.

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 14 years ago

    "Benjamin Maggi" <benjaminmaggi@gmail.com> wrote in message

    news:2118566303.579701308860038421.JavaMail.jive@flcspu-csapp-01.premierfarnell.com...

    Hi All,

     

    Im trying to create an 8 Layer PCB stackup I want to follow the best

    practices and I fond this site: http://www.hottconsultants.com along with

    many other that say that my 8 layer board stackup should be make like this

    (for better EMC and signal integrity)

     

    ~~~~~~~~~~~~~~~ Mounting Pads/Low Freq. Signals

    :::::::::::::::::::::::::::::: Prepreg

    +++++++++++++++ Pwr.

    =============== FR4 Core

    *------------------------------ * Gnd.

    :::::::::::::::::::::::::::::: Prepreg

    ~~~~~~~~~~~~~~~ High Freq. Signals

    =============== FR4 Core

    ~~~~~~~~~~~~~~~ High Freq. Signals

    :::::::::::::::::::::::::::::: Prepreg

    *------------------------------ * Gnd.

    =============== FR4 Core

    +++++++++++++++ Pwr.

    :::::::::::::::::::::::::::::: Prepreg

    ~~~~~~~~~~~~~~~ Low Freq. Signals/Test Pads

     

    I've never worked with eagle with so many layers, and never even bother

    with blind and burried vias.

    I need some help to define this stackup in eagle and also to create the

    throu, burried and blind vias to connect the layers.

     

    This is the very basic stackup I've with no vias

    image

    Image:eagle.jpg

     

    Goto DRC (gui button), choose layers tab and enter: (12+345*67*16) in

    setup box. Now you have the basics. You may enter layer thickness, but it

    doesnt have much value unless you use microvias.

    I have other prefs to signal assignment tho, but that all depends on usage

    (signal types, speeds,...). This setup may have a lot of crosstalk between

    inner layers if you route same direction, and power next to gnd is a waste

    of silent planes imho.

    I could give my suggestion if you say a bit more about the electronics you

    want on it.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 14 years ago in reply to Former Member

    Hello Morten,

     

    Thank you very much for your feedback.

     

    The project I'm trying to develop is quite simply.

     

    On one side of the board I've several shunt current sensors and on the other side I've a buffered output through a 74HC244 (tied to +5v) each of it's 8 outputs puts out a PWM frequency that is proportional to the current measured through the ADC, the range is not very high, from 0 to 1Mhz.

     

    On the top you should see a step-down converter which works at around 15khz, and a bunch of other peripherals, SPI, UART, LED's.

     

    On the center I've a microchip PIC33 doing all the hard work, clocked with a 20Mhz CX.

     

    Initially I wanted just 4 layers, but I'm considering stepping it up to 8 to for better signal integrity and EMC, and because my 4 layer is a total mess!

     

    A good designed could do the job with a 2 layer board, but not me, a good side effect of the 8 layer is better signal integrity and EMC characteristics and also I want better control of my routing so that I can scale up the prototype.

     

    Using only through plated vias would be fine (1+2*3+4*5+6*7+16) I guess. the result is:

    image

     

    You can see the routing mess I've done in the picture:

    image

     

    Regards.

    Ben.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 14 years ago in reply to Former Member

    "Benjamin Maggi" <communitymanager@premierfarnell.com> wrote in message

    news:1794334828.581141308947556391.JavaMail.jive@flcspu-csapp-01.premierfarnell.com...

    Hello Morten,

     

    Thank you very much for your feedback.

     

    The project I'm trying to develop is quite simply.

     

    On one side of the board I've several shunt current sensors and on the

    other side I've a buffered output through a 74HC244 (tied to +5v) each of

    it's 8 outputs puts out a PWM frequency that is proportional to the

    current measured through the ADC, the range is not very high, from 0 to

    1Mhz.

     

    On the top you should see a step-down converter which works at around

    15khz, and a bunch of other peripherals, SPI, UART, LED's.

     

    On the center I've a microchip PIC33 doing all the hard work, clocked with

    a 20Mhz CX.

     

    Initially I wanted just 4 layers, but I'm considering stepping it up to 8

    to for better signal integrity and EMC, and because my 4 layer is a total

    mess!

     

    A good designed could do the job with a 2 layer board, but not me, a good

    side effect of the 8 layer is better signal integrity and EMC

    characteristics and also I want better control of my routing so that I can

    scale up the prototype.

     

    Using only through plated vias would be fine (1+234*567+16) I guess.

    the result is:

    Image:through.jpg

     

    You can see the routing mess I've done in the picture:

    Image:brd.jpg

     

    First, a big boooo to element14 for image convertion to NNTP. They should at

    least put an URL to the image on the root system.

     

    Second, yes this looks like a 4 or 6 layer job. A microchip at 20Mhz doesnt

    need very much routing care, but if you have buffers with very fast rise and

    fall times, you should consider using slower for better EMC compatibility.

    Also remember to put damper resistors on fast logic outputs. That stops a

    lot of HF radiation.

    I guess crosstalk isnt a big issue here at all, so I would just have one GND

    layer and one power (maybe 1 layer shared if you have two voltages). If you

    make the outer layers power (not exclusive;use polygons), you can bake in

    the signals on the 4 inner layers and in some cases allow a track on outer.

    Take care of exposed voltage pins when you make space for screws.

     

    Also, take extra care of ESD protection on all your IO's, + be careful with

    routing that critical switch mode regulator.

    Its also possible you should reposition the components so that all multiwire

    buses has a short distance, while single IO can go long distances.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 14 years ago in reply to Former Member

    "Benjamin Maggi" <communitymanager@premierfarnell.com> wrote in message

    news:1794334828.581141308947556391.JavaMail.jive@flcspu-csapp-01.premierfarnell.com...

    Hello Morten,

     

    Thank you very much for your feedback.

     

    The project I'm trying to develop is quite simply.

     

    On one side of the board I've several shunt current sensors and on the

    other side I've a buffered output through a 74HC244 (tied to +5v) each of

    it's 8 outputs puts out a PWM frequency that is proportional to the

    current measured through the ADC, the range is not very high, from 0 to

    1Mhz.

     

    On the top you should see a step-down converter which works at around

    15khz, and a bunch of other peripherals, SPI, UART, LED's.

     

    On the center I've a microchip PIC33 doing all the hard work, clocked with

    a 20Mhz CX.

     

    Initially I wanted just 4 layers, but I'm considering stepping it up to 8

    to for better signal integrity and EMC, and because my 4 layer is a total

    mess!

     

    A good designed could do the job with a 2 layer board, but not me, a good

    side effect of the 8 layer is better signal integrity and EMC

    characteristics and also I want better control of my routing so that I can

    scale up the prototype.

     

    Using only through plated vias would be fine (1+234*567+16) I guess.

    the result is:

    Image:through.jpg

     

    You can see the routing mess I've done in the picture:

    Image:brd.jpg

     

    First, a big boooo to element14 for image convertion to NNTP. They should at

    least put an URL to the image on the root system.

     

    Second, yes this looks like a 4 or 6 layer job. A microchip at 20Mhz doesnt

    need very much routing care, but if you have buffers with very fast rise and

    fall times, you should consider using slower for better EMC compatibility.

    Also remember to put damper resistors on fast logic outputs. That stops a

    lot of HF radiation.

    I guess crosstalk isnt a big issue here at all, so I would just have one GND

    layer and one power (maybe 1 layer shared if you have two voltages). If you

    make the outer layers power (not exclusive;use polygons), you can bake in

    the signals on the 4 inner layers and in some cases allow a track on outer.

    Take care of exposed voltage pins when you make space for screws.

     

    Also, take extra care of ESD protection on all your IO's, + be careful with

    routing that critical switch mode regulator.

    Its also possible you should reposition the components so that all multiwire

    buses has a short distance, while single IO can go long distances.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data