Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) New user frustrated - can't find part  :(
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 14 replies
  • Subscribers 189 subscribers
  • Views 2396 views
  • Users 0 members are here
  • eagle
Related

New user frustrated - can't find part  :(

e14 Contributor
e14 Contributor over 15 years ago

Hi,

 

I just purchased Eagle CAD to draw a schematic for a project that was dumped in my lap.  Not only am I brand new to eagle but I'm also not experienced with electronics; I know enough to get basic stuff done, but oftens not enough to fully understand why it works (or doesn't)! image

 

So I've isntalled Eagle, watched tutorials, read the manual (I really did) and googled for various answers.  I STILL cannot figure out where to find a part to represent a 74HCT4514.  I've found parts that seem similar (e.g. 45xx > 4514 > 4514D) but the pin labels don't match what I'm expected (specifically, where is /E and /LE?)  The part in eagle has /ST and /INH however I'm unfamiliar with these labels.

 

Of the 6 hours I've spent ACTUALLY drawing a schematic I would say that 90% of that time has been spent search for parts.  I checked the eagle site for downloadable libraries but didn't see anything that seemed better than what is already installed.

 

Can someone please let me know if there is a pin compatible part in eagle for a 74HC4514?  If I DO have the correct part already, what do /ST and /INH stand for?

 

Thanks for reading,

Steve

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    Am 25.08.2011 08:13, schrieb Steve Klett:

    Hi,

     

    I just purchased Eagle CAD to draw a schematic for a project that was dumped in my lap.  Not only am I brand new to eagle but I'm also not experienced with electronics; I know enough to get basic stuff done, but oftens not enough to fully understand why it works (or doesn't)! image

     

    So I've isntalled Eagle, watched tutorials, read the manual (I really did) and googled for various answers.  I STILL cannot figure out where to find a part to represent a 74HCT4514.  I've found parts that seem similar (e.g. 45xx>  4514>  4514D) but the pin labels don't match what I'm expected (specifically, where is /E and /LE?)  The part in eagle has /ST and /INH however I'm unfamiliar with these labels.

     

    Of the 6 hours I've spent ACTUALLY drawing a schematic I would say that 90% of that time has been spent search for parts.  I checked the eagle site for downloadable libraries but didn't see anything that seemed better than what is already installed.

     

    Can someone please let me know if there is a pin compatible part in eagle for a 74HC4514?  If I DO have the correct part already, what do /ST and /INH stand for?

     

    Thanks for reading,

    Steve

     

     

    If you don't have a basic knowledge about ic-groups then you certainly

    have problems. Usually the groups are pin compatible, but here in my

    example I shall LIE a little bit to make things more clear (I hope).

    The name of the ic is 4514 but there are a lot of different groups

    like cd4514, 74ls4514, 74als4514, 47hc4514 or 74hct4514 etc.

    So you better get the datasheet for YOUR ic and check if it is compatible.

    The datasheet also tells you what the pins (/ST and /inh in your

    question) are doing.

    Neither eagle nor any other layout program gives you the garantee that

    its libraries are correct. It's allways up to you, so get the datasheets.

    And, since we are on it, the download site of cadsoft offers a lot of

    libraries and other stuff uploaded by users but no guarantee.

     

    For a beginning in a new sheet perhaps shou should enter in the command

    line(at the very top): "use *" without the " which means use ALL libraries.

     

    If you start to ADD devices, in this dialog at the very bottom left

    side, you find a search line marked with an "X".

    Here you can enter: 4514* to search for ALL parts that beginn with 4514.

    I hope you know the use of "?" and "*" and the combination of it.

     

    It is useless to search for EXACT the ic you want to have, because the

    libraries would blow up to gigabytes if every variation and character is

    listed and for all those still the different packages.

    So allways search for the basic number.

     

    Hopefully this helps you to enjoy eagle image

     

     

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    > If you don't have a basic knowledge about ic-groups then you certainly

    > have problems.

     

    I agree, it does make things more difficult.

     

    > So you better get the datasheet for YOUR ic and check if it is compatible.

    > The datasheet also tells you what the pins (/ST and /inh in your question)

    > are doing.

     

    I have all the datasheets for my parts, but Texas Instruments, NXP, etc. do not use the pin references that I'm seeing in Eagle - this is where my confusion comes in.  I don't mind comparing pins from datasheets but I don't even know which part Eagle is using for the 4514.

     

    > For a beginning in a new sheet perhaps shou should enter in the command

    > line(at the very top): "use *" without the " which means use ALL libraries.

    > If you start to ADD devices, in this dialog at the very bottom left

    > side, you find a search line marked with an "X".

    > Here you can enter: 4514* to search for ALL parts that beginn with 4514.

    > I hope you know the use of "?" and "*" and the combination of it.

     

    Yes, I've been using the wildcard in my searches and have tried to find a 4514 in the HC or HCT group but there doesn't appear to be one.

     

    > Hopefully this helps you to enjoy eagle

    It has helped me understand that I may need to create my own parts.  However this is not something I was expecting to need to do so I may consider hiring someone to take on this project for me.  Thanks for taking the time to respond to me in such detail, I appreciate it.

     

    -Steve

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Steve Klett schrieb:

     

    Yes, I've been using the wildcard in my searches and have tried to

    find a 4514 in the HC or HCT group but there doesn't appear to be

    one.

     

    You don't need to find it explicitly as HC or HCT. All those devices are

    pin and function compatible between "normal" CD series and 74HC/HCT

    series. Simply use any 4514 in the correct package and assign it the

    needed VALUE.

     

    It is generally helpful to think more generically about parts. As an

    example, I don't use devices for particular operational amplifiers or

    comparators - I just have a generic device (i.e. OP2) containing two

    opamps in the standard pinout and with all common package variants, and

    then I assign the particular values. Same for transistors, thyristors,

    triacs etc. - all parts with common standard pinouts can be defined

    generically. (Of course you need to take care that the desired part

    really uses that standard pinout... But then, when specifying a circuit,

    you need to take care anyway.)

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Guest wrote:

     

    ...It is generally helpful to think more generically about parts. As an

    example, I don't use devices for particular operational amplifiers or

    comparators - I just have a generic device (i.e. OP2) containing two

    opamps in the standard pinout and with all common package variants, and

    then I assign the particular values. Same for transistors, thyristors,

    triacs etc. - all parts with common standard pinouts can be defined

    generically. (Of course you need to take care that the desired part

    really uses that standard pinout... But then, when specifying a circuit,

    you need to take care anyway.) ...

     

     

    This is a good strategy and seems tthat it would save time, thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Guest wrote:

     

    ...It is generally helpful to think more generically about parts. As an

    example, I don't use devices for particular operational amplifiers or

    comparators - I just have a generic device (i.e. OP2) containing two

    opamps in the standard pinout and with all common package variants, and

    then I assign the particular values. Same for transistors, thyristors,

    triacs etc. - all parts with common standard pinouts can be defined

    generically. (Of course you need to take care that the desired part

    really uses that standard pinout... But then, when specifying a circuit,

    you need to take care anyway.) ...

     

     

    This is a good strategy and seems tthat it would save time, thanks.