Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) New user frustrated - can't find part  :(
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 14 replies
  • Subscribers 189 subscribers
  • Views 2394 views
  • Users 0 members are here
  • eagle
Related

New user frustrated - can't find part  :(

e14 Contributor
e14 Contributor over 15 years ago

Hi,

 

I just purchased Eagle CAD to draw a schematic for a project that was dumped in my lap.  Not only am I brand new to eagle but I'm also not experienced with electronics; I know enough to get basic stuff done, but oftens not enough to fully understand why it works (or doesn't)! image

 

So I've isntalled Eagle, watched tutorials, read the manual (I really did) and googled for various answers.  I STILL cannot figure out where to find a part to represent a 74HCT4514.  I've found parts that seem similar (e.g. 45xx > 4514 > 4514D) but the pin labels don't match what I'm expected (specifically, where is /E and /LE?)  The part in eagle has /ST and /INH however I'm unfamiliar with these labels.

 

Of the 6 hours I've spent ACTUALLY drawing a schematic I would say that 90% of that time has been spent search for parts.  I checked the eagle site for downloadable libraries but didn't see anything that seemed better than what is already installed.

 

Can someone please let me know if there is a pin compatible part in eagle for a 74HC4514?  If I DO have the correct part already, what do /ST and /INH stand for?

 

Thanks for reading,

Steve

  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to todd12

    On 11/12/2016 11:45 AM, tom dismond wrote:

    That is the same problem I have, but I'm looking for FDS2734 (or

    IRF7820PBFIRF7820PBFDo you have any suggestions

     

    Create the part for yourself. It's not hard, and it's the only way to be

    sure that the part is correct for your use. This is a pretty trivial

    device, and almost any Eagle tutorial will walk you through the process.

     

    Depending on some random library part is generally a bad idea. Even for

    something as trivial as a SMD resistor there are different suggested pad

    dimensions depending on whether the board will be assembled via wave

    soldering vs reflow.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • todd12
    0 todd12 over 9 years ago

    That is the same problem I have but I'm looking for FDS2734(or  IRF7820PBFIRF7820PBF Do you have any suggestions

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Steve Klett schrieb:

     

    Guest wrote:

    >

    > ..(The source is sometimes mentioned in the description of a device).

    > ...

    I've come across this on a few parts avnd immediately

    appreciated it.  I have created a few parts (8 resistor SOIC array

    and Clare CPC1014 SSR) and added links to the parts, manf. info and

    PN.  If everyone did this (where applicable) it would be nice

    image

     

    You should really consider using a newsreader or at least a working

    gateway to access these newsgroups. These posts via element14 are

    horrible to read.

     

    If you prefer web access, please have a look at eaglecentral.ca.

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Guest wrote:

     

    ... something like that (or, even nicer, would contain an overstrike,

    which now can be done in EAGLE by using '!EN').

     

     

     

    Cool, good tip, thanks!  I like the overstrike notation.  Also your advice to check the datasheet is good advice, thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Guest wrote:

     

    ...(The source is sometimes mentioned in the description of a device). ...

     

    I've come across this on a few parts avnd immediately appreciated it.  I have created a few parts (8 resistor SOIC array and Clare CPC1014 SSR) and added links to the parts, manf. info and PN.  If everyone did this (where applicable) it would be nice  image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Guest wrote:

     

    ...It is generally helpful to think more generically about parts. As an

    example, I don't use devices for particular operational amplifiers or

    comparators - I just have a generic device (i.e. OP2) containing two

    opamps in the standard pinout and with all common package variants, and

    then I assign the particular values. Same for transistors, thyristors,

    triacs etc. - all parts with common standard pinouts can be defined

    generically. (Of course you need to take care that the desired part

    really uses that standard pinout... But then, when specifying a circuit,

    you need to take care anyway.) ...

     

     

    This is a good strategy and seems tthat it would save time, thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Am 26.08.2011 03:40, schrieb Steve Klett:

    And hey! - they use "strobe" for /LE and "Inhibit" for /E (assuming they are pin compatible)

     

    For digital ICs, one VERY often names a pin after its function, assuming

    that this function is activated by a logic '1' signal.

    E.g., the input pin 'EN' might mean 'enable' and usually enables some

    functionality if connected to a logic '1'. If this function were

    activated by a logic '0', the pin would often be called 'EN\' or '/EN'

    or something like that (or, even nicer, would contain an overstrike,

    which now can be done in EAGLE by using '!EN').

     

    Depending on your view of the world, the same function could therefore

    be called either 'EN' (enabled with a logic '1') or '/DIS' (disabled

    with a logic '0'),...

     

    In your case, it would be '/E' (enabled with a logic '0') and 'INH'

    (inhibited or disabled with a logic '1'), which is essentially the same.

    However this may be, you can never fully rely on it, and always should

    risk a look into the data sheet.

     

    Andreas Weidner

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Am 26.08.2011 03:40, schrieb Steve Klett:

    You mention "Inhibit not" which I still need to read up on because the datasheet just says "inhibit"  From reading the datasheet it sounds like the outputs will respond to the inputs when the inhibit is LOW, so maybe this is what "inhibit not" means; "inhibit low"?

     

    Yes that means low level active image Unfortunately, as you have found

    out, different manufacturers use different identifiers. So one must

    compare the pin numbers. You see for cadsoft it is not so easy to hit

    the "correct" identifier, since there is none. It just depends what

    datasheet they used.

    (The source is sometimes mentioned in the description of a device).

    I have more than 4000 datasheets and still have to check a douzen or so

    against other manufacturers because those sheets contain insufficient

    information.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Steve Klett schrieb:

     

    Yes, I've been using the wildcard in my searches and have tried to

    find a 4514 in the HC or HCT group but there doesn't appear to be

    one.

     

    You don't need to find it explicitly as HC or HCT. All those devices are

    pin and function compatible between "normal" CD series and 74HC/HCT

    series. Simply use any 4514 in the correct package and assign it the

    needed VALUE.

     

    It is generally helpful to think more generically about parts. As an

    example, I don't use devices for particular operational amplifiers or

    comparators - I just have a generic device (i.e. OP2) containing two

    opamps in the standard pinout and with all common package variants, and

    then I assign the particular values. Same for transistors, thyristors,

    triacs etc. - all parts with common standard pinouts can be defined

    generically. (Of course you need to take care that the desired part

    really uses that standard pinout... But then, when specifying a circuit,

    you need to take care anyway.)

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Hi, thanks for the reply.  I realize there are multiple manufacturers but wasn't aware they would use different pin identifiers.

    Interesting - I just did a digikey search for "HC4514" to get a list of some manufacturers to include in this response.  I noticed fairchild down at the bottom and checked out their datasheet.  And hey! - they use "strobe" for /LE and "Inhibit" for /E (assuming they are pin compatible)

     

    You mention "Inhibit not" which I still need to read up on because the datasheet just says "inhibit"  From reading the datasheet it sounds like the outputs will respond to the inputs when the inhibit is LOW, so maybe this is what "inhibit not" means; "inhibit low"?

     

    Anyway, thanks for the response and information.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>