Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) New user frustrated - can't find part  :(
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 14 replies
  • Subscribers 189 subscribers
  • Views 2396 views
  • Users 0 members are here
  • eagle
Related

New user frustrated - can't find part  :(

e14 Contributor
e14 Contributor over 15 years ago

Hi,

 

I just purchased Eagle CAD to draw a schematic for a project that was dumped in my lap.  Not only am I brand new to eagle but I'm also not experienced with electronics; I know enough to get basic stuff done, but oftens not enough to fully understand why it works (or doesn't)! image

 

So I've isntalled Eagle, watched tutorials, read the manual (I really did) and googled for various answers.  I STILL cannot figure out where to find a part to represent a 74HCT4514.  I've found parts that seem similar (e.g. 45xx > 4514 > 4514D) but the pin labels don't match what I'm expected (specifically, where is /E and /LE?)  The part in eagle has /ST and /INH however I'm unfamiliar with these labels.

 

Of the 6 hours I've spent ACTUALLY drawing a schematic I would say that 90% of that time has been spent search for parts.  I checked the eagle site for downloadable libraries but didn't see anything that seemed better than what is already installed.

 

Can someone please let me know if there is a pin compatible part in eagle for a 74HC4514?  If I DO have the correct part already, what do /ST and /INH stand for?

 

Thanks for reading,

Steve

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    Am 25.08.2011 08:13, schrieb Steve Klett:

    but the pin labels don't match what I'm expected (specifically, where is /E and /LE?)  The part in eagle has /ST and /INH

     

    A lot of parts are available from MORE than one manufacturer, and,

    unfortunately, these sometimes name their component pins differently:

     

    E.g., the pin called LE ('latch enable') might be called /INH ('inhibit

    not') by some other manufacturer. Without looking into the data sheets,

    it's sometimes tricky to get to know whether things are compatible or

    not. This might or might not be the case with your IC, but at least it's

    something you should be aware of.

     

    Andreas Weidner

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Hi, thanks for the reply.  I realize there are multiple manufacturers but wasn't aware they would use different pin identifiers.

    Interesting - I just did a digikey search for "HC4514" to get a list of some manufacturers to include in this response.  I noticed fairchild down at the bottom and checked out their datasheet.  And hey! - they use "strobe" for /LE and "Inhibit" for /E (assuming they are pin compatible)

     

    You mention "Inhibit not" which I still need to read up on because the datasheet just says "inhibit"  From reading the datasheet it sounds like the outputs will respond to the inputs when the inhibit is LOW, so maybe this is what "inhibit not" means; "inhibit low"?

     

    Anyway, thanks for the response and information.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Am 26.08.2011 03:40, schrieb Steve Klett:

    And hey! - they use "strobe" for /LE and "Inhibit" for /E (assuming they are pin compatible)

     

    For digital ICs, one VERY often names a pin after its function, assuming

    that this function is activated by a logic '1' signal.

    E.g., the input pin 'EN' might mean 'enable' and usually enables some

    functionality if connected to a logic '1'. If this function were

    activated by a logic '0', the pin would often be called 'EN\' or '/EN'

    or something like that (or, even nicer, would contain an overstrike,

    which now can be done in EAGLE by using '!EN').

     

    Depending on your view of the world, the same function could therefore

    be called either 'EN' (enabled with a logic '1') or '/DIS' (disabled

    with a logic '0'),...

     

    In your case, it would be '/E' (enabled with a logic '0') and 'INH'

    (inhibited or disabled with a logic '1'), which is essentially the same.

    However this may be, you can never fully rely on it, and always should

    risk a look into the data sheet.

     

    Andreas Weidner

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Guest wrote:

     

    ... something like that (or, even nicer, would contain an overstrike,

    which now can be done in EAGLE by using '!EN').

     

     

     

    Cool, good tip, thanks!  I like the overstrike notation.  Also your advice to check the datasheet is good advice, thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Guest wrote:

     

    ... something like that (or, even nicer, would contain an overstrike,

    which now can be done in EAGLE by using '!EN').

     

     

     

    Cool, good tip, thanks!  I like the overstrike notation.  Also your advice to check the datasheet is good advice, thanks.