EAGLE User Support (English) New user frustrated - can't find part  :(
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
  • State Not Answered
  • Replies 14 replies
  • Subscribers 181 subscribers
  • Views 1999 views
  • Users 0 members are here
  • eagle
Related

New user frustrated - can't find part  :(

Former Member
Former Member over 14 years ago

Hi,

 

I just purchased Eagle CAD to draw a schematic for a project that was dumped in my lap.  Not only am I brand new to eagle but I'm also not experienced with electronics; I know enough to get basic stuff done, but oftens not enough to fully understand why it works (or doesn't)! image

 

So I've isntalled Eagle, watched tutorials, read the manual (I really did) and googled for various answers.  I STILL cannot figure out where to find a part to represent a 74HCT4514.  I've found parts that seem similar (e.g. 45xx > 4514 > 4514D) but the pin labels don't match what I'm expected (specifically, where is /E and /LE?)  The part in eagle has /ST and /INH however I'm unfamiliar with these labels.

 

Of the 6 hours I've spent ACTUALLY drawing a schematic I would say that 90% of that time has been spent search for parts.  I checked the eagle site for downloadable libraries but didn't see anything that seemed better than what is already installed.

 

Can someone please let me know if there is a pin compatible part in eagle for a 74HC4514?  If I DO have the correct part already, what do /ST and /INH stand for?

 

Thanks for reading,

Steve

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 14 years ago in reply to Former Member

    Guest wrote:

     

    ... something like that (or, even nicer, would contain an overstrike,

    which now can be done in EAGLE by using '!EN').

     

     

     

    Cool, good tip, thanks!  I like the overstrike notation.  Also your advice to check the datasheet is good advice, thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 14 years ago in reply to Former Member

    Steve Klett schrieb:

     

    Guest wrote:

    >

    > ..(The source is sometimes mentioned in the description of a device).

    > ...

    I've come across this on a few parts avnd immediately

    appreciated it.  I have created a few parts (8 resistor SOIC array

    and Clare CPC1014 SSR) and added links to the parts, manf. info and

    PN.  If everyone did this (where applicable) it would be nice

    image

     

    You should really consider using a newsreader or at least a working

    gateway to access these newsgroups. These posts via element14 are

    horrible to read.

     

    If you prefer web access, please have a look at eaglecentral.ca.

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • todd12
    0 todd12 over 9 years ago

    That is the same problem I have but I'm looking for FDS2734(or  IRF7820PBFIRF7820PBF Do you have any suggestions

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to todd12

    On 11/12/2016 11:45 AM, tom dismond wrote:

    That is the same problem I have, but I'm looking for FDS2734 (or

    IRF7820PBFIRF7820PBFDo you have any suggestions

     

    Create the part for yourself. It's not hard, and it's the only way to be

    sure that the part is correct for your use. This is a pretty trivial

    device, and almost any Eagle tutorial will walk you through the process.

     

    Depending on some random library part is generally a bad idea. Even for

    something as trivial as a SMD resistor there are different suggested pad

    dimensions depending on whether the board will be assembled via wave

    soldering vs reflow.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<