Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Shared access to schematic/project
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 2 answers
  • Subscribers 188 subscribers
  • Views 533 views
  • Users 0 members are here
  • eagle
  • question
Related

Shared access to schematic/project

e14 Contributor
e14 Contributor over 14 years ago

Hi,

 

I have hired a contractor to do some eagle work for me as I'm not yet up to speed enough to meet a deadline.  Anyway, so I'd still like to help and be involved in the process but I don't see how the two of us can work on the same file without creating a real mess.  I can solve the shared access issue by granting him VPN to our file server, but I highly doubt that eagle will be too happy if we both are editing the file at the same time.  THe only option I can think of is to use version control or a basic "Are you working right now?  No? OK, then I will for awhile and will email you when I'm done" type approach.

 

Anyone here who works or has worked in a multiuser scenario have any tips for me?

 

Thanks for reading,

Steve

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    On 09/02/2011 12:41 AM, Steve Klett wrote:

    Hi,

     

    I have hired a contractor to do some eagle work for me as I'm not yet up to speed enough to meet a deadline.  Anyway, so I'd still like to help and be involved in the process but I don't see how the two of us can work on the same file without creating a real mess.  I can solve the shared access issue by granting him VPN to our file server, but I highly doubt that eagle will be too happy if we both are editing the file at the same time.  THe only option I can think of is to use version control or a basic "Are you working right now?  No? OK, then I will for awhile and will email you when I'm done" type approach.

     

    Anyone here who works or has worked in a multiuser scenario have any tips for me?

     

    Thanks for reading,

    Steve

     

    I have not done it and it is not going to be easy. Before you have a

    board linked to the schematic you should be able to work on different

    pages then cut and paste from one version to the other. Keep detailed

    log of notes of what you are changing and adding and why.

    If you are going to change default net names it may make merging data

    require a little more overhead. If so you should keep a master net name

    list.

    Once you are in the layout phase you have to keep both sch and brd open.

    From this point on simultaneous editing should be locked out.

     

    Paul R

     

     

     

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    On 09/02/2011 12:41 AM, Steve Klett wrote:

    Hi,

     

    I have hired a contractor to do some eagle work for me as I'm not yet up to speed enough to meet a deadline.  Anyway, so I'd still like to help and be involved in the process but I don't see how the two of us can work on the same file without creating a real mess.  I can solve the shared access issue by granting him VPN to our file server, but I highly doubt that eagle will be too happy if we both are editing the file at the same time.  THe only option I can think of is to use version control or a basic "Are you working right now?  No? OK, then I will for awhile and will email you when I'm done" type approach.

     

    Anyone here who works or has worked in a multiuser scenario have any tips for me?

     

    Thanks for reading,

    Steve

     

    I have not done it and it is not going to be easy. Before you have a

    board linked to the schematic you should be able to work on different

    pages then cut and paste from one version to the other. Keep detailed

    log of notes of what you are changing and adding and why.

    If you are going to change default net names it may make merging data

    require a little more overhead. If so you should keep a master net name

    list.

    Once you are in the layout phase you have to keep both sch and brd open.

    From this point on simultaneous editing should be locked out.

     

    Paul R