Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Shared access to schematic/project
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 2 answers
  • Subscribers 188 subscribers
  • Views 533 views
  • Users 0 members are here
  • eagle
  • question
Related

Shared access to schematic/project

e14 Contributor
e14 Contributor over 14 years ago

Hi,

 

I have hired a contractor to do some eagle work for me as I'm not yet up to speed enough to meet a deadline.  Anyway, so I'd still like to help and be involved in the process but I don't see how the two of us can work on the same file without creating a real mess.  I can solve the shared access issue by granting him VPN to our file server, but I highly doubt that eagle will be too happy if we both are editing the file at the same time.  THe only option I can think of is to use version control or a basic "Are you working right now?  No? OK, then I will for awhile and will email you when I'm done" type approach.

 

Anyone here who works or has worked in a multiuser scenario have any tips for me?

 

Thanks for reading,

Steve

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    On 09/02/2011 12:41 AM, Steve Klett wrote:

    Hi,

     

    I have hired a contractor to do some eagle work for me

    ...

    I don't see how the two of us

    can work on the same file without creating a real mess.

     

    You can't.  You need to designate a single owner of the files.

     

    THe only option I can think of is to use

    version control

     

    Yep.  This is the best solution.  We use Perforce in our shop.  You can

    get a free version limited to 2 users.  Other change management systems

    should work as well.

     

    "Are you working right now?  No? OK, then

    I will for awhile and will email you when I'm done" type approach.

     

    Yep.  It's generally called "baton passing", taken from a relay race

    where one runner passes a baton to the next.  Whoever holds the baton

    owns the files.

     

    With all that said, Cadsoft is planning to store files in an XML format,

    though I'm not sure what version in which this is scheduled to be

    implemented.  At one point I heard 6.0.  Regardless, an ascii text

    format like XML should make it easier to merge multiple changes.

     

    Enjoy,

        - Chuck

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    On 09/02/2011 12:41 AM, Steve Klett wrote:

    Hi,

     

    I have hired a contractor to do some eagle work for me

    ...

    I don't see how the two of us

    can work on the same file without creating a real mess.

     

    You can't.  You need to designate a single owner of the files.

     

    THe only option I can think of is to use

    version control

     

    Yep.  This is the best solution.  We use Perforce in our shop.  You can

    get a free version limited to 2 users.  Other change management systems

    should work as well.

     

    "Are you working right now?  No? OK, then

    I will for awhile and will email you when I'm done" type approach.

     

    Yep.  It's generally called "baton passing", taken from a relay race

    where one runner passes a baton to the next.  Whoever holds the baton

    owns the files.

     

    With all that said, Cadsoft is planning to store files in an XML format,

    though I'm not sure what version in which this is scheduled to be

    implemented.  At one point I heard 6.0.  Regardless, an ascii text

    format like XML should make it easier to merge multiple changes.

     

    Enjoy,

        - Chuck

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks Chuck.  I've ended up basically "staying out of it" and when I have something to contribute I send a small mini-schematic as a separate file.  it's worked out well.